flexio_biss_sync_transfer#
Overview#
The flexio_biss_sync example shows how to use flexio BiSS driver in sync way:
In this example, a flexio simulated BiSS connect to the encoder through RS-485, the board will send requests to and receive responses from the board.
Supported Boards#
FRDM-MIMXRT1186
Hardware requirements
USB Type-C cable
FRDM-IMXRT1186 board
5V power supply
Personal Computer
FRDM-LVPMSM-FA board
Board settings
This example requires connecting between FRDM-IMXRT1186 board and FRDM-LVPMSM-FA board.
Short J300-1 and J300-2 on the FRDM-LVPMSM-FA board
FRDM-LVPMSM-FA SW90[1-4] = 1001
FRDM-LVPMSM-FA SW30[1-4] = 0100
FRDM-LVPMSM-FA J70-1 -> VCC pin of encoder
FRDM-LVPMSM-FA J70-6 -> GND pin of encoder
FRDM-LVPMSM-FA J70-2 -> CLK+ pin of encoder
FRDM-LVPMSM-FA J70-7 -> CLK- pin of encoder
FRDM-LVPMSM-FA J70-3 -> Data+ pin of encoder
FRDM-LVPMSM-FA J70-8 -> Data- pin of encoder
Prepare the Demo
Connect a USB Type-C cable between the PC host and the OpenSDA USB port on the FRDM-IMXRT1186 board.
Connect 5V power supply, then switch SW5 to power on the FRDM-IMXRT1186 board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
Encoder BiSS example
FlexIO Root Clock is 80 MHz
The initial frame format:
head=4; mt=12; st=16; erWr=2; crc=6; stop=1; cdm=4; data=30; total=41; whole=45
CDM Value = FFFFFFFFFC02AAAA
[OK] Shifer1 = 0xB7C46BA0; Shifter0 = 0x00001C50
head=8; mt=12; st=16; erWr=2; crc=6; stop=1; cdm=4; data=30; total=45; whole=49
##### ******************** Running the loop test ********************
Shifer1 = 0x7C46BA20; Shifter0 = 0x0001C50B
CRC = 0x11; CRC_Cal = 0x11
head = 0xE2
CRCdata = 0x216F88D7
ST = 0x0000E235
##### MT = 0x085B
Shifer1 = 0x7C46BA20; Shifter0 = 0x0001C50B
CRC = 0x11; CRC_Cal = 0x11
head = 0xE2
CRCdata = 0x216F88D7
ST = 0x0000E235
MT = 0x085B