MCUXpresso SDK Documentation

acmp_interrupt

acmp_interrupt#

Overview#

The sw_trig example demostrated how to use BCTU software trigger function to trigger the ADC to convert.

Supported Boards#

FRDM-MCXE31B
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXE318 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

BCTU SoftWare Trigger Example
Please press any key to get the ADC value
ADC channel 48 value: 12021
ADC channel 48 value: 12019
ADC channel 48 value: 12022
FRDM-MCXE32B
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXE318 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

BCTU SoftWare Trigger Example
Please press any key to get the ADC value
ADC channel 48 value: 12021
ADC channel 48 value: 12019
ADC channel 48 value: 12022