lpc_adc_basic#
Overview#
The lpc_adc_basic example shows how to use LPC ADC driver in the simplest way.
In this example, the sensor is used to created the input analog signal. When user type in any key from the keyboard, the software trigger API is called to start the conversion. Then it polls the conversion sequence A’s flag till the conversion is completed. When the conversion is completed, just print the conversion result to terminal.
Project Information#
1.what are ADC conversion sequences? A conversion sequence is a single pass through a series of A/D conversions performed on a selected set of A/D channels. Software can set-up two independent conversion sequences, either of which can be triggered by software or by a transition on one of the hardware triggers. Each sequence can be triggered by a different hardware trigger. One of these conversion sequences is referred to as the A sequence and the other as the B sequence. It is not necessary to employ both sequences. An optional single-step mode allows advancing through the channels of a sequence one at a time on each successive occurrence of a trigger. The user can select whether a trigger on the B sequence can interrupt an already-in-progress A sequence. The B sequence, however, can never be interrupted by an A trigger.
How to use software-triggered conversion? There are two ways that software can trigger a conversion sequence:
Start Bit: The first way to software-trigger an sequence is by setting the START bit in the corresponding SEQn_CTRL register. The response to this is identical to occurrence of a hardware trigger on that sequence. Specifically, one cycle of conversions through that conversion sequence will be immediately triggered except as indicated above. (In this example, we use this way.)
Burst Mode: The other way to initiate conversions is to set the BURST bit in the SEQn_CTRL register. As long as this bit is 1 the designated conversion sequence will be continuously and repetitively cycled through. Any new software or hardware trigger on this sequence will be ignored.
Program Flow#
1.This example demonstrates how to configure the A sequences with polling, assigning one channel with software trigger, you can configure channel via “DEMO_ADC_SAMPLE_CHANNEL_NUMBER”.
2.Before configuration of the ADC begins, the ADC is put through a self-calibration cycle.
3.After ADC channels are assigned to each of the sequences, the software trigger is chosen. Setting SEQA_CTRL_START to ‘1’ will trigger sequence A.
4.After ADC channels are assigned to each of the sequences, if the user enters any key via terminal, software trigger will start.
5.Read the corresponding DATAVALID field with polling to judge whether the conversion completes and the result is ready. If the result is ready, the example will printf result information to terminal.
Supported Boards#
LPC845BREAKOUT
Hardware requirements
Micro USB cable
LPC845 Breakout board
Personal Computer
Board settings
ADC CH0 input signal 32(PIO0-7).
Prepare the demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Adjust the potentiometer and press any key from keyboard to trigger the conversion. The log below shows the output of the ADC basic driver example in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
...
LPCXpresso51U68
Hardware requirements
Mini/micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings
ADC CH4 input signal J1-15(PIO1-1).
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Press any key from keyboard and trigger the conversion. The log below shows example output of the ADC basic example in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
...
LPCXpresso54628
Hardware requirements
Micro USB cable
LPCXpresso54628 board
Personal Computer
Board settings
ADC CH4 input signal J12-2(PIO0-16).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Press any key from keyboard and trigger the conversion. The log below shows example output of the ADC basic example in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
...
LPCXpresso54S018
Hardware requirements
Micro USB cable
LPCXpresso54S018 board
Personal Computer
Board settings
ADC CH4 input signal J12-2(PIO0-16).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
Press any key from keyboard and trigger the conversion. The log below shows example output of the ADC basic example in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
...
LPCXpresso54S018M
Hardware requirements
Micro USB cable
LPCXpresso54S018M board
Personal Computer
Board settings
ADC CH4 input signal J12-2(PIO0-16).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018M.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
Press any key from keyboard and trigger the conversion. The log below shows example output of the ADC basic example in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 4
adcResultInfoStruct.overrunFlag = 0
...
LPCXpresso802
Toolchain supported
IAR embedded Workbench 8.11.3
Keil MDK 5.23
MCUXpresso10.1.0
Hardware requirements
Micro USB cable
LPCXpresso54608 board
Personal Computer
Board settings
ADC CH8 input signal CN5-10(PIO0-15).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 8
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 8
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 8
adcResultInfoStruct.overrunFlag = 0
...
Customization options
LPCXpresso804
Toolchain supported
IAR embedded Workbench 8.22.1
Keil MDK 5.24a
MCUXpresso10.2.0
Hardware requirements
Micro USB cable
LPCXpresso804 board
Personal Computer
Board settings
ADC CH7 input signal CN6-11(PIO0-10).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 7
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 7
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 7
adcResultInfoStruct.overrunFlag = 0
...
Customization options
LPCXpresso824MAX
Toolchain supported
IAR embedded Workbench 8.11.3
Keil MDK 5.23
MCUXpresso10.1.0
Hardware requirements
Micro USB cable
LPCXpresso824MAX board
Personal Computer
Board settings
ADC CH1 input signal J5-1(PIO0-6).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J3) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 1
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 1
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 1
adcResultInfoStruct.overrunFlag = 0
...
Customization options
LPCXpresso845MAX
Toolchain supported
IAR embedded Workbench 8.11.3
Keil MDK 5.23
MCUXpresso10.1.0
Hardware requirements
Micro USB cable
LPCXpresso54608 board
Personal Computer
Board settings
ADC CH0 input signal J1-6(PIO0-7).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC basic example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 676
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
adcResultInfoStruct.result = 675
adcResultInfoStruct.channelNumber = 0
adcResultInfoStruct.overrunFlag = 0
...
Customization options
LPCXpresso860MAX
Toolchain supported
IAR embedded Workbench 8.11.3
Keil MDK 5.23
MCUXpresso10.1.0
Hardware requirements
Micro USB cable
LPCXpresso860MAX board
Personal Computer
Board settings
ADC CH0 input signal J6-12(PIO0-7).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J4) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Monitor the information on the debug console.
Expected Result
Press any key and print user channel’s result in serial terminal.