ZPS_tsAplZdpNodeDescStoreRsp#
This structure is used to store Node_Desc_store_rsp message data - a response to a call to the function ZPS_eAplZdpNodeDescStoreRequest(). This response indicates whether the sending node has successfully stored the received Node descriptor in its primary discovery cache.
The ZPS_tsAplZdpNodeDescStoreRspstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpNodeDescStoreRsp;
where u8Statusis the return status for ZPS_eAplZdpNodeDescStoreRequest().
Parent topic:ZDP response structures