MCUXpresso SDK Documentation

iap3_flash_fcb

iap3_flash_fcb#

Overview#

The IAP flash project is a simple demonstration program of the SDK IAP driver. such as using a complete FlexSPI NOR Configuration Block to configure the flash, erasing sectors and programing pages. All operations are followed by flash memory check to ensure the data operated are successful.

Supported Boards#

EVK-MIMXRT595
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the example in the terminal window:

IAP flash example started!

***NOR Flash Initialization Success!***

***NOR Flash Erase Success!***

***NOR Flash All Pages Read/Write Success!***
EVK-MIMXRT685
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the iap_flash_fcb example in the terminal window:

IAP flash example started!

***NOR Flash Initialization Success!***

***NOR Flash Erase Success!***

***NOR Flash All Pages Read/Write Success!***
MIMXRT685-AUD-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the iap_flash_fcb example in the terminal window:

IAP flash example started!

***NOR Flash Initialization Success!***

***NOR Flash Erase Success!***

***NOR Flash All Pages Read/Write Success!***