lpflexcomm_interrupt_transfer#
Overview#
The lpflexcomm_interrupt_transfer example shows how to use lpi2c driver and lpuart driver to build a interrupt based application.In this example,
lpi2c and lpuart use same lpflexcomm instance.
Supported Boards#
FRDM-MCXN236
Hardware requirements
Type-C USB cable
FRDM-MCXN236 board
Personal Computer
Board settings
To make LPFLEXCOMM example work, connections needed to be as follows:
LPI2C3 SCL(J2-12) --> LPI2C2 SCL(J5-5)
LPI2C3 SDA(J2-8) --> LPI2C2 SDA(J5-6)
LPUART3 TX(J2-10) --> LPUART2 RX(J1-2)
LPUART3 RX(J2-6) --> LPUART2 TX(J1-4)
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPFLEXCOMM example.
In this example 2 lpflexcomm instances are used.
First the lpflexcomm instances are used as I2C, I2C master of instance 1 sends data to I2C slave of instance2.
Then the lpflexcomm instances are used as UART, UART2 sends data back to UART1.
The next round UART1 sends data to UART2, then lpflexcomm instances switch back to I2C mode,
I2C master of instance 1 reads data from I2C slave of instance 2 of the data received as UART.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will send data using LPI2C --- MASTER TO SLAVE
Transfer all data matched!
Slave received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 2 TO instance 1
Transfer all data matched!
Master received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 1 TO instance 2
Transfer all data matched!
Slave received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPI2C --- SLAVE TO MASTER
Transfer all data matched!
Master received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
DEMO END!
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
To make LPFLEXCOMM example work, connections needed to be as follows:
LPI2C1 SCL(J2-12) --> LPI2C2 SCL(J2-20)
LPI2C1 SDA(J2-8) --> LPI2C2 SDA(J2-18)
LPUART1 TX(J2-10) --> LPUART2 RX(J1-2)
LPUART1 RX(J2-6) --> LPUART2 TX(J1-4)
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPFLEXCOMM example.
In this example 2 lpflexcomm instances are used.
First the lpflexcomm instances are used as I2C, I2C master of instance 1 sends data to I2C slave of instance2.
Then the lpflexcomm instances are used as UART, UART2 sends data back to UART1.
The next round UART1 sends data to UART2, then lpflexcomm instances switch back to I2C mode,
I2C master of instance 1 reads data from I2C slave of instance 2 of the data received as UART.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will send data using LPI2C --- MASTER TO SLAVE
Transfer all data matched!
Slave received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 2 TO instance 1
Transfer all data matched!
Master received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 1 TO instance 2
Transfer all data matched!
Slave received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPI2C --- SLAVE TO MASTER
Transfer all data matched!
Master received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
DEMO END!
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
Board settings
To make LPFLEXCOMM example work, connections needed to be as follows:
LPI2C1 SCL(J2-12) --> LPI2C2 SCL(J2-20)
LPI2C1 SDA(J2-8) --> LPI2C2 SDA(J2-18)
LPUART1 TX(J2-10) --> LPUART2 RX(J1-2)
LPUART1 RX(J2-6) --> LPUART2 TX(J1-4)
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPFLEXCOMM example.
In this example 2 lpflexcomm instances are used.
First the lpflexcomm instances are used as I2C, I2C master of instance 1 sends data to I2C slave of instance2.
Then the lpflexcomm instances are used as UART, UART2 sends data back to UART1.
The next round UART1 sends data to UART2, then lpflexcomm instances switch back to I2C mode,
I2C master of instance 1 reads data from I2C slave of instance 2 of the data received as UART.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will send data using LPI2C --- MASTER TO SLAVE
Transfer all data matched!
Slave received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 2 TO instance 1
Transfer all data matched!
Master received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 1 TO instance 2
Transfer all data matched!
Slave received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPI2C --- SLAVE TO MASTER
Transfer all data matched!
Master received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
DEMO END!
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
To make LPFLEXCOMM example work, connections needed to be as follows:
LPI2C1 SCL(J2-12) --> LPI2C2 SCL(J2-20)
LPI2C1 SDA(J2-8) --> LPI2C2 SDA(J2-18)
LPUART1 TX(J2-10) --> LPUART2 RX(J1-2)
LPUART1 RX(J2-6) --> LPUART2 TX(J1-4)
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPFLEXCOMM example.
In this example 2 lpflexcomm instances are used.
First the lpflexcomm instances are used as I2C, I2C master of instance 1 sends data to I2C slave of instance2.
Then the lpflexcomm instances are used as UART, UART2 sends data back to UART1.
The next round UART1 sends data to UART2, then lpflexcomm instances switch back to I2C mode,
I2C master of instance 1 reads data from I2C slave of instance 2 of the data received as UART.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will send data using LPI2C --- MASTER TO SLAVE
Transfer all data matched!
Slave received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 2 TO instance 1
Transfer all data matched!
Master received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 1 TO instance 2
Transfer all data matched!
Slave received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPI2C --- SLAVE TO MASTER
Transfer all data matched!
Master received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
DEMO END!
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
To make LPFLEXCOMM example work, connections needed to be as follows:
LPI2C1 SCL(J2-12) --> LPI2C2 SCL(J2-20)
LPI2C1 SDA(J2-8) --> LPI2C2 SDA(J2-18)
LPUART1 TX(J2-10) --> LPUART2 RX(J1-2)
LPUART1 RX(J2-6) --> LPUART2 TX(J1-4)
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPFLEXCOMM example.
In this example 2 lpflexcomm instances are used.
First the lpflexcomm instances are used as I2C, I2C master of instance 1 sends data to I2C slave of instance2.
Then the lpflexcomm instances are used as UART, UART2 sends data back to UART1.
The next round UART1 sends data to UART2, then lpflexcomm instances switch back to I2C mode,
I2C master of instance 1 reads data from I2C slave of instance 2 of the data received as UART.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will send data using LPI2C --- MASTER TO SLAVE
Transfer all data matched!
Slave received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 2 TO instance 1
Transfer all data matched!
Master received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPUART --- instance 1 TO instance 2
Transfer all data matched!
Slave received data by LPUART:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Will reply data using LPI2C --- SLAVE TO MASTER
Transfer all data matched!
Master received data by LPI2C:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
DEMO END!