dsc_mscan_loopback#
Overview#
The mscan_loopback_functional example shows how to use the loopback test mode to debug your CAN Bus design:
To demonstrates this example, only one board is needed. The example will configure one MSCAN Message Tx buffer and Rx buffer with same ID. After that, the example will send a CAN Message from the Tx Buffer to the Rx Buffer throuth internal loopback interconnect and print out the Message payload to terminal.
Supported Boards#
TWR-MC56F8200
Hardware requirements
Mini USB cable
TWR-MC56F8200 board
Personal Computer
Board hardware common setting
HW reworkd(workaround):
Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.
Power setting:
Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2
UART setting:
Connect J8 pin3 and pin4 Connect J9 pin3 and pin4
Onboard OSJTAG debugger setting:
Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open
Board settings
No special settings are required.
Prepare the Demo
Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with OSJTAG debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
==MSCAN loopback functional example -- Start.==
Send message!
tx word0 = 0x12345678
tx word1 = 0x87654321
Received message!
rx word0 = 0x12345678
rx word1 = 0x87654321
==MSCAN loopback functional example -- Finish.==