niobe4analog_mem_interface#
Overview#
The mem_interface project is a simple demonstration program of the SDK IAP driver. It erases and programs a portion of internal and external flash memory. A message a printed on the UART terminal as various operations on flash memory are performed.
Supported Boards#
LPCXpresso55S36
Hardware requirements
Mini/micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Internal flash example start:
Calling API_Version!
IAP API version = x.x.x
Calling API_Init!
API_Init Successfully!
PFlash Information:
Program Flash Base Address: xx
Total Program Flash Size: xx
Program Flash Sector Size: xx
Erasing internal flash
Successfully erased internal flash xx -> xx
Calling MEM_Write to program internal flash!
Successfully Programmed and Verified Location xx -> xx
End of internal flash example!