MCUXpresso SDK Documentation

dsc_edma_memory_to_memory

dsc_edma_memory_to_memory#

Overview#

The EDMA memory to memory example is a simple demonstration program that uses the SDK software. It excuates one shot transfer from source buffer to destination buffer using the SDK EDMA drivers. The purpose of this example is to show how to use the EDMA and to provide a simple example for debugging and further development.

Supported Boards#

MC56F80000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F80000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2

  2. Reset pin setting:

    Connect J11 pin2 and pin3

  3. Debugger setting:

    Connect J13 pin 1-2, 3-4, 5-6, 7-8

Board settings

No special settings are required.

Prepare the Demo
  1. Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with Multilink debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA memory to memory example begin.



Destination Buffer:

0   0   0   0



EDMA memory to memory example finish.



Destination Buffer:

1   2   3   4
MC56F81000-EVK
Hardware requirements
  • 2 x Micro USB cable

  • MC56F81000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J8 pin2 and pin3 Connect J5 pin1 and pin2 Connect J6 pin1 and pin2

  2. Onboard PnE U-MultiLink debugger setting:

    Connet J11 pin2 and pin3 Connect J13 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger PnE U-MultiLink. Note: when use external debugger(connected to J10), leave all J13 pins open.

Board settings

No special settings are required.

Prepare the Demo
  1. Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.

  2. Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board with PnE U-MultiLink debug configuration.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted default FCF(flash configuration field) makes the MCU boot from flash.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA memory to memory example begin.



Destination Buffer:

0   0   0   0



EDMA memory to memory example finish.



Destination Buffer:

1   2   3   4
MC56F83000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F83000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J19 pin2 and pin3 Connect J12 pin1 and pin2 Connect J13 pin1 and pin2 Connect J15 pin1 and pin2 Connect J16 pin2 and pin3 Connect J17 pin1 and pin2

  2. Onboard OSJTAG debugger setting:

    Leave J5 open Leave J6 open Note: J6 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J11 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J10), leave all J11 pins open.

Board settings

No special settings are required.

Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J8) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted that default FCF(flash configuration field) setting makes MCU boot from bootloader. So after reset button press, it will wait 5s(wait in bootloader) to run the application code.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA memory to memory example begin.



Destination Buffer:

0   0   0   0



EDMA memory to memory example finish.



Destination Buffer:

1   2   3   4