MCUXpresso SDK Documentation

sctimer_simple_pwm

sctimer_simple_pwm#

Overview#

The SCTimer project is a simple demonstration program of the SDK SCTimer’s driver capabiltiy to generate PWM signals. The SCTimer project enables a 32-bit counter to output two center-aligned PWM signals with parameters set to 24kHz frequency. The duty cycles of the two PWM signals are 50% and 20%, respectively.

Supported Boards#

EVK-MIMXRT595
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings

No special settings are required.

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

Use Oscilloscope to measure and observe the J30-1, J30-2 output signal.

EVK-MIMXRT685
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings

No special settings are required.

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

Use Oscilloscope to measure and observe the TP6/7 output signal.

FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT4    		J3-3 (P1_22)
SCT0_OUT5    		J1-8 (P1_23)
Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J17) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on J3-3 and J1-8 using an oscilloscope.

FRDM-MCXN947T
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947T board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT4    		J3-3 (P1_22)
SCT0_OUT5    		J1-8 (P1_23)
Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J17) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on J3-3 and J1-8 using an oscilloscope.

FRDM-MCXW23
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW23 Board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT4    		J2-6
SCT0_OUT5    		J2-7 
Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

Probe an oscilloscope to the output pins described in board settings, you will see two PWM signals.

FRDM-RW612
Hardware requirements
  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

No special settings are required.

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

Use Oscilloscope to measure and observe the J5-4, J1-1 output signal.

LPC845BREAKOUT
Hardware requirements
  • Micro USB cable

  • LPC845 Breakout board

  • Personal Computer

Board settings

No special settings are required.

Prepare the demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board.

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope
LPCXpresso51U68
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso51U68 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope
LPCXpresso54628
Hardware requirements
  • Micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope
  • Probe oscilloscope at J13-5 and J13-16 to see output signal.

LPCXpresso54S018
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:

  1. Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”

      This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
    
  2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

    a. Open SEGGER J-FLASH Lite, select device LPC54S018.

    b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

    c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
    The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope
  • Probe oscilloscope at J13-5 and J13-16 to see output signal.

LPCXpresso54S018M
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018M board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:

  1. Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”

      This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
    
  2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

    a. Open SEGGER J-FLASH Lite, select device LPC54S018M.

    b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

    c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
    The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope
  • Probe oscilloscope at J13-5 and J13-16 to see output signal.

LPCXpresso55S06
Hardware requirements
  • Micro USB cable

  • LPCXpresso55S06 board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT2    		J12-12
SCT0_OUT6    		J12-17
Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on J12_12 and J12_17 using an oscilloscope.

LPCXpresso55S16
Hardware requirements
  • Micro USB cable

  • LPCXpresso55S16 board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT2    		J12-12
SCT0_OUT6    		J12-14

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on J12_12 and J12_14 using an oscilloscope.

LPCXpresso55S28
Hardware requirements
  • Micro USB cable

  • LPCXpresso55S28 board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT2    		P18-11
SCT0_OUT6    		P18-13 
# Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (P6) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on P18_11 and P18_13 using an oscilloscope.

LPCXpresso55S36
Hardware requirements
  • Micro USB cable

  • LPCXpresso55S36 board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT0    		J10-5 (P1_4)
SCT0_OUT4    		J10-13(P1_17)
Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on J10-5 and J10-13 using an oscilloscope.

LPCXpresso55S69
Hardware requirements
  • Micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT2    		P18-11
SCT0_OUT6    		P18-13 
# Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (P6) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on P18_11 and P18_13 using an oscilloscope.

LPCXpresso824MAX
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso824MAX board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope
LPCXpresso845MAX
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso845MAX board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope
MCX-N5XX-EVK
Hardware requirements
  • Micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT4    		J3-3 (P1_22)
SCT0_OUT5    		J1-8 (P1_23)
Prepare the Demo
  1. Connect a micro USB cable between the host PC and the MCU-Link USB port (J5) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on J3-3 and J1-8 using an oscilloscope.

MCX-N9XX-EVK
Hardware requirements
  • Micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT4    		J3-3 (P1_22)
SCT0_OUT5    		J1-8 (P1_23)
Prepare the Demo
  1. Connect a micro USB cable between the host PC and the MCU-Link USB port (J5) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

You’ll see center-aligned PWM signals on J3-3 and J1-8 using an oscilloscope.

MIMXRT685-AUD-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings

No special settings are required.

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

Use Oscilloscope to measure and observe the JP30-1, JP30-2 output signal.

RD-RW612-BGA
Hardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings

No special settings are required.

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

Use Oscilloscope to measure and observe the HD2 Pin4, Pin5 output signal.

MCXW23-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings
Output signal		Board location
SCT0_OUT4    		J20-5
SCT0_OUT5   		J20-6
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope

Probe an oscilloscope to the output pins described in board settings, you will see two PWM signals.