MCUXpresso SDK Documentation

ZPS_tsAplZdpNwkAddrRsp

ZPS_tsAplZdpNwkAddrRsp#

This structure is used to store NWK_addr_rsp message data - a response to a call to the function ZPS_eAplZdpNwkAddrRequest(). This response contains the network address of the node with a given IEEE address.

The ZPS_tsAplZdpNwkAddrRspstructure is detailed below.

typedef struct { uint8 u8Status;
     uint64 u64IeeeAddrRemoteDev;
     uint16 u16NwkAddrRemoteDev;
     uint8 u8NumAssocDev;
     uint8 u8StartIndex;
     /* Rest of the message is variable Length */
     uint16* pNwkAddrAssocDevList;
} ZPS_tsAplZdpNwkAddrRsp;

where:

  • u8Statusis the return status for ZPS_eAplZdpNwkAddrRequest()

  • u64IeeeAddrRemoteDevis the IEEE address of the remote node that sent the response (this is the IEEE address specified in the original request)

  • u16NwkAddrRemoteDevis the network address of the remote node that sent the response (this is the network address that was requested)

  • u8NumAssocDevis the number of neighboring nodes for which network addresses are also being reported (in the remainder of the structure)

  • u8StartIndexis the index in the remote node’s Neighbor table of the first entry to be included in this report. This element should be ignored if the element u8NumAssocDevis 0.

  • pNwkAddrAssocDevListis a pointer to a list of 16-bit network addresses of the remote node’s neighbors (this is a variable-length list with four bytes per node). This element should be ignored if the element u8NumAssocDevis 0.

Parent topic:ZDP response structures