freertos_lpi2c#
Overview#
The LPI2C Example project is a demonstration program that uses the KSDK software to manipulate the Low Power Inter- Integrated Circuit. The example uses two instances of LPI2C, one in configured as master and the other one as slave. The LPI2C master sends data to LPI2C slave. The slave will check the data it receives and shows the log.
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below. Single Board:
LPI2C example -- MasterInterrupt_SlaveInterrupt.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
I2C master transfer completed successfully.
I2C slave transfer completed successfully.
Transfer successfully!
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Board to Board: Master side
LPI2C example -- MasterInterrupt_SlaveInterrupt.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
I2C master transfer completed successfully.
Slave side:
LPI2C example -- MasterInterrupt_SlaveInterrupt.
I2C slave transfer completed successfully.
Transfer successfully!
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f