ZPS_tsAplZdpBackupSourceBindRsp
This structure is used to store Backup_Source_Bind_rsp message data - a response to a call to the function ZPS_eAplZdpBackupSourceBindRequest(). This response indicates the status of the back-up request.
The ZPS_tsAplZdpBackupSourceBindRspstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpBackupSourceBindRsp;
where u8Statusis the return status for the function ZPS_eAplZdpBackupSourceBindRequest().
Parent topic:ZDP response structures