lwip_httpsrv_enet_qos_freertos#
Overview#
The lwip_httpsrv demo application demonstrates an HTTP server on the lwIP TCP/IP stack with bare metal SDK or FreeRTOS. The user uses an Internet browser to send a request for connection. The board acts as an HTTP server and sends a webpage back to the PC.
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1170-EVKB board
Personal Computer
Board settings
No special settings are required.
FRDM-IMXRT1152
Hardware requirements
FRDM-IMXRT1152 board
USB Type-C cable
RJ45 network cable
Personal Computer
Board settings
Connect the USB Type-C cable to the FRDM-IMXRT1152 USB debug connector.
Use the 10/100 Ethernet RJ45 port (J112).
Set J134 to position 1-2 for the shared
ENET_MDIOrouting.Set J136 to position 1-2 for the
ENET_QOS_REF_CLK1routing.
FRDM-MCXE31B
Hardware requirements
USB-C cable
Network cable RJ45 standard
FRDM-MCXE31B board
Personal Computer
Board settings
No special settings are required.