pmc_temperature_sensor#
Overview#
The demo shows how to measure the temperature within the PMC module.
In this demo, the ADC input channel is mapped to an internal temperature sensor. When running the project, typing any key into debug console would trigger a series of ADC conversions. When the conversions are done, the temperature is calculated per the specific formula.
Supported Boards#
EVK-MCIMX7ULP
Hardware requirements
Micro USB cable
MCIMX7ULP-EVK board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a micro USB cable between the host PC and the J6 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
The log below shows the output of the demo in the terminal window:
PMC Temperature Sensor Demo
ADC Full Range: 4096
Please press any key to get temperature from the internal temperature sensor.
Current temperature: 32.59
Current temperature: 32.67
EVK-MIMXRT595
Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
PMC Temperature Sensor Demo
ADC Full Range: 4096
Please press any key to get temperature from the internal temperature sensor.
Current temperature: 28.59
Current temperature: 28.67
MIMXRT700-EVK
Hardware requirements
Micro USB cable
Target board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-LINK USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
PMC Temperature Sensor Demo
ADC Full Range: 65536
Please press any key to get temperature from the internal temperature sensor.
Current temperature: 28.59
Current temperature: 28.67
FRDM-IMXRT700
Hardware requirements
Type-C USB cable
FRDM-IMXRT700 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the PC host and the MCU-LINK USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
PMC Temperature Sensor Demo
ADC Full Range: 65536
Please press any key to get temperature from the internal temperature sensor.
Current temperature: 28.59
Current temperature: 28.67