MCUXpresso SDK Documentation

spi_interrupt

Contents

spi_interrupt#

Overview#

The spi_interrupt example shows how to use spi functional API to do interrupt transfer:

In this example, one spi instance as master and another spi instance as slave. Master sends a piece of data to slave, and check if the data slave received is correct.