rtc_freerunning# Overview# The RTC project is a simple demonstration program of the SDK RTC driver. The test will set the RTC free running interrupt threshold to be the 32K value and free running interrupt will occur every one second.