MCUXpresso SDK Documentation

lpadc_dma

lpadc_dma#

Overview#

The lpadc_dma example shows how to use ADC to trigger a DMA transfer.

In this example, user should indicate a channel to provide a voltage signal (can be controlled by user) as the LPADC’s sample input. When running the project, typing any key into debug console would trigger the conversion, the software trigger API is called to start the conversion. When the ADC conversion is completed, it would trigger the DMA in ping-pong transfer mode to move the ADC conversion result from ADC conversion data register to user indicated memory. Then the main loop waits for the transfer to be done and print the latest ADC conversion word and ADC conversion value average to terminal.

Supported Boards#

EVK-MIMXRT595
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings
  • Input voltage signal(0~1.8V) to J30-1(LPADC0 CH0).

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, following information can be seen on the terminal:

LPADC DMA Example

ADC Full Range: 4096

Full channel scale (Factor of 1).

Please press any key to trigger the conversion.

Adc conversion word : 0x81006148

ADC conversion value: 3113

Adc conversion word : 0x81006140

ADC conversion value: 3112

Adc conversion word : 0x81006140

ADC conversion value: 3112
EVK-MIMXRT685
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings
  • Set VREF_L to GND, VREF_H to 1.8V (connect JP9, JP10).

  • Input voltage signal(0~1.8V) to J30-1(LPADC0 CH0).

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, following information can be seen on the terminal:

LPADC DMA Example

ADC Full Range: 4096

Full channel scale (Factor of 1).

Please press any key to trigger the conversion.

Adc conversion word : 0x81006148

ADC conversion value: 3113

Adc conversion word : 0x81006140

ADC conversion value: 3112

Adc conversion word : 0x81006140

ADC conversion value: 3112
LPCXpresso55S06
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso55S06 board

  • Personal Computer

Board settings
  • ADC CH0A input signal J13-3(PIO0_23).

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the lpadc dma example in the terminal window:

LPADC DMA Example

ADC Full Range: 65536

Please press any key to trigger the conversion.

Adc conversion word : 0x81008BA1

ADC conversion value: 35745

Adc conversion word : 0x81008BE7

ADC conversion value: 35815

Adc conversion word : 0x81008B14

ADC conversion value: 35604

LPCXpresso55S16
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso55s16 board

  • Personal Computer

Board settings
  • ADC CH0A input signal J13-3(PIO0_23). The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the lpadc dma example in the terminal window:

LPADC DMA Example

ADC Full Range: 65536

Please press any key to trigger the conversion.

Adc conversion word : 0x81008BA1

ADC conversion value: 35745

Adc conversion word : 0x81008BE7

ADC conversion value: 35815

Adc conversion word : 0x81008B14

ADC conversion value: 35604

LPCXpresso55S36
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso55S36 board

  • Personal Computer

Board settings
  • ADC CH0A input signal J7-1(PIO1_9).

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the lpadc dma example in the terminal window:

LPADC DMA Example

ADC Full Range: 65536

Please press any key to trigger the conversion.

Adc conversion word : 0x81008BA1

ADC conversion value: 35745

Adc conversion word : 0x81008BE7

ADC conversion value: 35815

Adc conversion word : 0x81008B14

ADC conversion value: 35604

LPCXpresso55S69
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings
  • Connect a jumper to P15-2 and P15-3.

  • ADC CH0A input signal P28-1(PIO0-23).

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the lpadc dma example in the terminal window:

LPADC DMA Example

ADC Full Range: 4096

Full channel scale (Factor of 1).

Please press any key to trigger the conversion.

Adc conversion word : 0x81006148

ADC conversion value: 3113

Adc conversion word : 0x81006140

ADC conversion value: 3112

Adc conversion word : 0x81006140

MIMXRT685-AUD-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings
  • Set VREF_L to GND, VREF_H to 1.8V (connect JP9, JP10).

  • Input voltage signal(0~1.8V) to LPADC0 CH0 (R405, P_5_ADC0_0 side)

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, following information can be seen on the terminal:

LPADC DMA Example

ADC Full Range: 4096

Full channel scale (Factor of 1).

Please press any key to trigger the conversion.

Adc conversion word : 0x81006148

ADC conversion value: 3113

Adc conversion word : 0x81006140

ADC conversion value: 3112

Adc conversion word : 0x81006140

ADC conversion value: 3112