MCUXpresso SDK Documentation

ZPS_tsAplZdpBackupBindTableRsp

ZPS_tsAplZdpBackupBindTableRsp#

This structure is used to store Backup_Bind_Table_rsp message data - a response to a call to the function ZPS_eAplZdpBackupBindTableRequest(). This response indicates the status of the back-up request.

The ZPS_tsAplZdpBackupBindTableRspstructure is detailed below.

typedef struct {
    uint8 u8Status;
    uint16 u16EntryCount;
} ZPS_tsAplZdpBackupBindTableRsp;

where:

  • u8Statusis the return status for ZPS_eAplZdpBackupBindTableRequest()

  • u16EntryCountis the number of binding table entries that have been backed up

Parent topic:ZDP response structures