MCUXpresso SDK Documentation

enc_index_interrupt

enc_index_interrupt#

Overview#

The enc_index_interrupt example shows how to use the interrupt of ENC module with ENC driver.

In this example, user needs to connect a real encoder to the board. Actually, only PHASE A and PHASE B are enough for the basic application. However, the additional INDEX/HOME/TRIGGER could be used as the event detector.

INDEX: This pulse can optionally reset the position counter and the pulse accumulator of the quadrature decoder module. It also causes a change of state on the revolution counter. The direction of this change, increment or decrement, is calculated from the PHASEA and PHASEB inputs.

HOME: This input can be used to trigger the initialization of the position counters. Often this signal is connected to a sensor signalling the motor or machine, sending notification that it has reached a defined home position.

TRIGGER: This input can be used to clear the position counters or to take a snapshot of the POS, REV, and POSD registers. Often this signal is connected to a periodic pulse generator or timer to indicate an elapsed time period.

This example uses INDEX to response the external event. When running the project, user can turn the encoder so that ENC module can monitor the position change. Also, a variable counter would count the time of INDEX interrupt for rising edge on INDEX signal line.

Running the demo#

Turn the encoder feed the negative pulse into INDEX and type in any key into terminal. When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

ENC INDEX Interrupt Example. Press any key to get the encoder values …

Current position value: 0 Current position differential value: 0 Current position revolution value: 0 g_EncIndexCounter: 0

Current position value: 20 Current position differential value: 20 Current position revolution value: 1 g_EncIndexCounter: 1

Current position value: 25 Current position differential value: 5 Current position revolution value: 2 g_EncIndexCounter: 2

Supported Boards#

EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J22.5 -> kXBARA1_InputIomuxXbarIn21 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J22.6 -> kXBARA1_InputIomuxXbarIn22 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J22.3 -> kXBARA1_InputIomuxXbarIn23 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J16.5 -> kXBARA1_InputIomuxXbarIn21 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J16.6 -> kXBARA1_InputIomuxXbarIn22 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J16.3 -> kXBARA1_InputIomuxXbarIn23 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J9.4 -> kXBARA1_InputIomuxXbarIn38 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J9.2 -> kXBARA1_InputIomuxXbarIn39 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J9.6 -> kXBARA1_InputIomuxXbarIn40 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J16.5 -> kXBARA1_InputIomuxXbarIn21 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J16.6 -> kXBARA1_InputIomuxXbarIn22 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J16.3 -> kXBARA1_InputIomuxXbarIn23 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-IMXRT1152
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1152 board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J44.10 -> kXBARA1_InputIomuxXbarIn04 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J44.12 -> kXBARA1_InputIomuxXbarIn05 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J44.14 -> kXBARA1_InputIomuxXbarIn06 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

EVK-MIMXRT1015
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1015 board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings

Remove D25

For pin connection between board and encoder J30-3 -> kXBARA1_InputIomuxXbarInout12 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J30-1 -> kXBARA1_InputIomuxXbarInout13 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB D25-C -> kXBARA1_InputIomuxXbarInout16 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings

Remove R59

For pin connection between board and encoder J17.2 -> kXBARA1_InputIomuxXbarInout12 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J17.1 -> kXBARA1_InputIomuxXbarInout13 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB U1F-46 -> kXBARA1_InputIomuxXbarInout16 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings

Remove R59

For pin connection between board and encoder J17.4 -> kXBARA1_InputIomuxXbarInout12 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J17.2 -> kXBARA1_InputIomuxXbarInout13 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB U1F-46 -> kXBARA1_InputIomuxXbarInout16 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J16.5 -> kXBARA1_InputIomuxXbarIn21 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J16.6 -> kXBARA1_InputIomuxXbarIn22 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J16.3 -> kXBARA1_InputIomuxXbarIn23 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J22.5 -> kXBARA1_InputIomuxXbarIn21 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J22.6 -> kXBARA1_InputIomuxXbarIn22 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J22.3 -> kXBARA1_InputIomuxXbarIn23 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J9.4 -> kXBARA1_InputIomuxXbarIn38 -> kXBARA1_OutputEnc1PhaseAInput -> ENC_PHA J9.2 -> kXBARA1_InputIomuxXbarIn39 -> kXBARA1_OutputEnc1PhaseBInput -> ENC_PHB J9.6 -> kXBARA1_InputIomuxXbarIn40 -> kXBARA1_OutputEnc1Index -> ENC_INDEX

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

LPCXpresso55S36
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso55S36 board

  • Personal Computer

  • An encoder with PHASE A/B signals, optionally with INDEX signal.

Board settings
  1. For pin connection between board and encoder, J10.3 -> kINPUTMUX_ExtTrigIn3ToEnc0Phasea -> ENC_PHA J10.1 -> kINPUTMUX_ExtTrigIn2ToEnc0Phaseb -> ENC_PHB J12.3 -> kINPUTMUX_ExtTrigIn8ToEnc0Index -> ENC_INDEX

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bits

    • No flow control

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.