dev_composite_hid_mouse_hid_keyboard#
Overview#
The application is a simple demonstration program based on the MCUXpresso SDK. The application is enumerated as HID-compliant mouse and keyboard devices.
System Requirement#
Hardware requirements#
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer (PC)
Software requirements#
The project files for lite version examples are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_composite_hid_mouse_hid_keyboard_lite/ / .
For non-lite version example, the files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_composite_hid_mouse_hid_keyboard/ / .
The
is Bare Metal or FreeRTOS OS.
Getting Started#
Hardware Settings#
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example#
Download the program to the target board.
Connect the target board to the external power source (the example is self-powered).
Power off the target board. And then power on again.
Connect a USB cable between the PC and the USB device port of the board.
For detailed instructions, see the appropriate board User’s Guide.
Run the example#
Plug in the device, which is running the composite example, into PC. An HID-compliant mouse and a keyboard are enumerated in the Device Manager.
For the HID mouse, the mouse arrow moving on the PC screen in the rectangular rotation.\n
For the HID keyboard, see the screen while scrolling up and down.
*/
Supported Boards#
LPCXpresso55S16
Getting Started
Hardware Settings
The Jumper settings:\n JP20 1-2, JP21 1-2 and JP22 1-2 for chip power.
FRDM-K32L2A4S
Getting Started
Hardware Settings
The Jumper settings:\n J9 1-2, J16 1-2.