MCUXpresso SDK Documentation

iap_basic

iap_basic#

Overview#

The IAP project is a simple demonstration program of the SDK IAP driver. It reads part id, boot code version, unique id and reinvoke ISP. A message a printed on the UART terminal as various bascial iap operations are performed.

Supported Boards#

LPC845BREAKOUT
Hardware requirements
  • Micro USB cable

  • LPCXpresso845 Breakout board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example

LPCXpresso54628
Hardware requirements
  • Micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example

LPCXpresso54S018
Hardware requirements
  • Micro USB cable

  • LPCXpresso54s018 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example

LPCXpresso54S018M
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018M board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example

LPCXpresso802
Hardware requirements
  • Micro USB cable

  • LPCXpresso802 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the CMSIS DAP port(CN1 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example

LPCXpresso804
Hardware requirements
  • Micro USB cable

  • LPCXpresso804 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the CMSIS DAP port(CN2 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example

LPCXpresso824MAX
Hardware requirements
  • Micro USB cable

  • LPCXpresso824MAX board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the CMSIS DAP port(J3 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example

LPCXpresso845MAX
Hardware requirements
  • Micro USB cable

  • LPCXpresso845MAX board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the CMSIS DAP port(J4 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example

LPCXpresso860MAX
Hardware requirements
  • Micro USB cable

  • LPCXpresso860MAX board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the CMSIS DAP port(J4 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo
  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP example

PartID: XXXXX

The major version is: XXXX

The minor version is: XXXX

Unique ID: XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

End of IAP Example