Getting Started with Package# Table of Contents Overview MCUXpresso SDK Board Support Package Folders Example application structure Locating example application source files Running a demo application using IAR Build an example application Run an example application Run a demo using MCUXpresso IDE Select the workspace location Build an example application Run an example application How to determine COM Port How to set the board to the Bootloader ISP mode Updating debugger firmware Updating NBU for Wireless Examples