itrc_1#
Overview#
The ITRC Example project is a demonstration program that uses the MCUX SDK software to set up Intrusion and Tamper Response Controller. Then tests the expected behaviour.
Running the demo#
When the demo runs successfully, the terminal displays similar information like the following:
ITRC Peripheral Driver Example
Pass: No Event/Action triggered after Init
Enable ITRC IRQ Action response to SW Event 0
Trigger SW Event 0
ITRC IRQ Reached!
ITRC STATUS0:
Software event 0 occurred!
ITRC triggered ITRC_IRQ output!
Clear ITRC IRQ and SW Event 0 STATUS
Disable ITRC IRQ Action response to SW Event 0
Trigger SW Event 0
Pass: No Action triggered after disabling
End of example
Supported Boards#
FRDM-RW612
Hardware requirements
Mini/micro USB cable
FRDM-RW612 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
RD-RW612-BGA
Hardware requirements
Mini/micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.