flexnvm_dflash#
Overview#
The flexnvm_dflash example shows how to use flash driver to operate data flash:
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
For parts with FlexNVM:
FlexNVM DFlash example Start
Flash is UNSECURE!
DFlash Information:
Data Flash Base Address: (xx)
Data Flash Total Size: xx KB, hex: (xx)
Data Flash Sector Size: xx KB, hex: (xx)
Erase a sector of Data Flash
Successfully Erased Sector xx -> xx
Program a buffer to a sector of Data Flash
Successfully Programmed and Verified Location xx -> xx
End of FlexNVM Dflash example
For Some parts Without FlexNVM (such as K65FN):
FlexNVM DFlash example Start
Current device doesn't support FlexNVM feature
End of FlexNVM Dflash example
Supported Boards#
FRDM-KE15Z
Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal
FlexNVM DFlash example Start
Flash is UNSECURE!
DFlash Information:
Data Flash Base Address: (xx)
Data Flash Total Size: xx KB, hex: (xx)
Data Flash Sector Size: xx KB, hex: (xx)
Erase a sector of Data Flash
Successfully Erased Sector xx -> xx
Program a buffer to a sector of Data Flash
Successfully Programmed and Verified Location xx -> xx
End of FlexNVM Dflash example
FRDM-MCXE247
Hardware requirements
Micro USB cable
FRDM-MCXE247 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and USB port on the target board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal
FlexNVM DFlash example Start
Flash is UNSECURE!
DFlash Information:
Data Flash Base Address: (xx)
Data Flash Total Size: xx KB, hex: (xx)
Data Flash Sector Size: xx KB, hex: (xx)
Erase a sector of Data Flash
Successfully Erased Sector xx -> xx
Program a buffer to a sector of Data Flash
Successfully Programmed and Verified Location xx -> xx
End of FlexNVM Dflash example