MCUXpresso SDK Documentation

emios_center_aligned_pwm

emios_center_aligned_pwm#

Overview#

The eMIOS project is a simple demonstration example of the SDK eMIOS driver to use eMIOS as PWM generator.
It configures eMIOS UC (Unified channel) as Center Aligned Output PWM with Dead Time Insertion Buffered (OPWMCB) mode.
This example generates three 10kHz center aligned PWM, there duty cycle are 50%, 25% and 12.5%.

Supported Boards#

FRDM-MCXE31B
Hardware requirements
  • Micro USB cable

  • FRDM-MCXE31B Board

  • Personal Computer

  • Oscilloscope

Board settings

Probe the PWM signal using an oscilloscope

  • At J3-15 for PWM channel 0

  • At J3-13 for PWM channel 1

  • At J3-11 for PWM channel 2

Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, following information can be seen on the OpenSDA terminal:

eMIOS center aligned PWM Example

FRDM-MCXE32B
Hardware requirements
  • Micro USB cable

  • FRDM-MCXE32B board

  • Personal Computer

  • Oscilloscope

Board settings

Probe the PWM signal using an oscilloscope

  • At J3-15 for PWM channel 0

  • At J3-13 for PWM channel 1

  • At J3-11 for PWM channel 2

Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, following information can be seen on the OpenSDA terminal:

eMIOS center aligned PWM Example