Complex Dependency
MCUXpresso SDK build system provides complex dependencies record and resolve for both sections(examples and components) and sources.
Section Level Dependency
Kconfig dependency mechanism and tool is used to describe and resolve section level dependency.
Dependency Mechanisms
Kconfig provides depends on, select and choice dependency mechanisms.
depends on
It defines a dependency for Kconfig symbol. If multiple dependencies are defined, they can be connected with
&&,||, and!for NOT.The Kconfig item won’t be showed if the
depends onis not satisfied.select
It forces a symbol to true which means the depended component is selected anyway no matter its dependency is satisfied or not.
choice
It defines a choice group. The single choice can only be of type bool or tristate. If no type is specified for a choice, its type will be determined by the type of the first choice element in the group or remain unknown if none of the choice elements have a type specified.
Kconfig processor will give detailed warnings about unsatisfied component selection so that you can immediately find it and update.
Practice Recommendation
For software components depending on hardware related dependency items like
board,device,device_id, please usedepends on. In this way, for any component whose hardware dependencies are not satisfied, it will not be showed so that not bloat the Kconfig GUI.For software components depending on software component, priority to use
select. It helps to auto select component dependency.For cycle dependency case like FOO needs to
selectBAR and BAR needs toselectFOO, since Kconfig doesn’t support cycle dependency, so you cannot use mutuallyselectbetween FOO and BAR. The recommendation is use bothselectanddepends on. For example, FOOselectBAR and BARdepends onFOO. In this way, when you tick FOO, then BAR will be automatically selected. When FOO dependency is not satisfied, BAR cannot be showed.If there are
any ofdependencies,choicecan satisfy the need.
Hardware Dependency Items
Following Harry dependency items are provided for components to depends on:
Dependency Item |
Illustration |
|---|---|
MCUX_HW_DEVICE_<device> |
Device, like MIMXRT1176 |
MCUX_HW_DEVICE_ID_<device_id> |
Device id, like MIMXRT1176xxxxx |
MCUX_HW_CORE_<core_name> |
Core name, like cm4f |
MCUX_HW_CORE_ID_<core_id> |
Core id, like cm4 |
MCUX_HW_BOARD_<board name> |
Board name, like evkbmimxrt1170 |
MCUX_HW_KIT_<kit name> |
Kit name, like mimxrt700evk_a8974 |
MCUX_HW_<fpu type> |
fpu type name, like MCUX_HW_FPV4_SP |
MCUX_HW_DSP |
DSP or no DSP |
MCUX_HW_MPU |
MPU or no MPU |
MCUX_HW_SAU |
Secure or nonsecure |
All these dependency items shall be defined in device Kconfig.chip.
Source Level Dependency
Source level dependency is achieved through the CMake extension, like
mcux_add_source(
SOURCES portable/GCC/ARM_CM0/port.c
# The following 2 lines mean port.c only supports cm0p core and toolchain armgcc, mcux and mdk
CORES cm0p
TOOLCHAINS armgcc mcux mdk
)
Please refer the mcux_add_source/mcux_add_include extension arguments for supported dependency items.