All_reset_but_netc reset trigger#
Overview#
The all_reset_but_netc reset trigger demo application demonstrates how to send the all_reset_but_netc reset quest.
Supported Boards#
IMX943-EVK
Hardware requirements
Micro USB cable
IMX943-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.
Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
The demo to trigger all_reset_but_netc reset starts.
Press S to send all_reset_but_netc reset request.