shell_mem#
Overview#
The Shell Demo application demonstrates ram and flash memory access commands.
Supported Boards#
EVK-MCIMX7ULP
Hardware requirements
Micro USB cable
MCIMX7ULP-EVK board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
The example is uses QSPI0. The module uses PTB8, PTB15 ~PTB19 pins. No special jumper needs to be connected.
Please note this application can’t support running with Linux BSP!
Please note that this application must be built with ram link file! Because if running the application in QSPI flash in place, the QSPI flash erase/program feature of the application might affect the instruction fetch. If QSPI execution in place(XIP) is really needed, please make sure the flash erase/program operation must be handled by RAM function and disable all interrupts to avoid jumping into interrupt handler in flash area during flash updating.
It’s better to use IAR to debug this application. If you use u-boot to copy the image file to the qspi please do not use “flasherase” and “flashwrite” command to do some opperation from the offset address 0x0 to 0x10000. This range is reserved for the application image.
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a micro USB cable between the host PC and the J6 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
NOTE: Don’t build this example with flash linkage file since this example need to modify QSPI controller, so program itself cannot be run in QSPI flash.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below. Use corresponding command to read and modify memory.
SHELL (build: Nov 25 2016)
Copyright (c) 2015 Freescale Semiconductor
SHELL>> help
"help": Lists all the registered commands
"exit": Exit program
"memget8 arg1 arg2": read memory in 8bit unit
Usage:
arg1: addr memory address
arg2: count memory read count
"memget16 arg1 arg2": read memory in 16bit unit
Usage:
arg1: addr memory address
arg2: count memory read count
"memget32 arg1 arg2": read memory in 32bit unit
Usage:
arg1: addr memory address
arg2: count memory unit read count
"memset8 arg1 arg2 arg3": write memory in 8bit unit
Usage:
arg1: addr memory address
arg2: value memory write value
arg3: count memory unit write count
"memset16 arg1 arg2 arg3": write memory in 16bit unit
Usage:
arg1: addr memory address
arg2: value memory write value
arg3: count memory unit write count
"memset32 arg1 arg2 arg3": write memory in 32bit unit
Usage:
arg1: addr memory address
arg2: value memory write value
arg3: count memory unit write count
"memcmp8 arg1 arg2 arg3": compare memory in 8bit unit
Usage:
arg1: addr1 memory address1
arg2: addr2 memory address2
arg3: count memory unit compare count
"memcmp16 arg1 arg2 arg3": compare memory in 16bit unit
Usage:
arg1: addr1 memory address1
arg2: addr2 memory address2
arg3: count memory unit compare count
"memcmp32 arg1 arg2 arg3": compare memory in 32bit unit
Usage:
arg1: addr1 memory address1
arg2: addr2 memory address2
arg3: count memory unit compare count
"memcpy8 arg1 arg2 arg3": copy memory in 8bit unit
Usage:
arg1: dst destination memory address
arg2: src source memory address
arg3: count memory unit copy count
"memcpy16 arg1 arg2 arg3": copy memory in 16bit unit
Usage:
arg1: dst destination memory address
arg2: src source memory address
arg3: count memory unit copy count
"memcpy32 arg1 arg2 arg3": copy memory in 32bit unit
Usage:
arg1: dst destination memory address
arg2: src source memory address
arg3: count memory unit copy count
"flasherase arg1 arg2": erase QSPI flash
Usage:
arg1: offset flash memory offset in bytes
arg2: bytes flash memory size in bytes
"flashwrite arg1 arg2 arg3": write QSPI flash
Usage:
arg1: addr source memory address
arg2: offset flash memory offset in bytes
arg3: bytes flash memory size in bytes
SHELL>>