powerquad_benchmark_matrix#
Overview#
This example shows the PowerQuad based CMSIS DSP function performance. It could be compared with the project powerquad_benckmark_sw_matrix to show the PowerQuad performance improvement.
Supported Boards#
EVK9-MIMX8ULP
Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the example with with imx-mkimage.(Not running it with your IDE, unless it will be failed to running). Note: After a successful execution, if you need to execute again, you need to completely power down the board and restart it again.
Running the demo
NOTE: Depending on the toolchain configuration, the benchmark result might be different.
BOARD_ReleaseTRDC: 75 start release trdc
BOARD_ReleaseTRDC: 78 finished release trdc, status = 0xd6
BOARD_SetTrdcGlobalConfig: 93 start setup trdc
BOARD_SetTrdcGlobalConfig: 402 finished setup trdc
CMSIS DSP benchmark matrix test start.
arm_mat_add_q15Test: xxx
arm_mat_add_q31Test: xxx
arm_mat_add_f32Test: xxx
arm_mat_sub_q15Test: xxx
arm_mat_sub_q31Test: xxx
arm_mat_sub_f32Test: xxx
arm_mat_mult_q15Test: xxx
arm_mat_mult_q31Test: xxx
arm_mat_mult_f32Test: xxx
arm_mat_inverse_f32Test: xxx
arm_mat_trans_q15Test: xxx
arm_mat_trans_q31Test: xxx
arm_mat_trans_f32Test: xxx
arm_mat_scale_q15Test: xxx
arm_mat_scale_q31Test: xxx
arm_mat_scale_f32Test: xxx
CMSIS DSP benchmark matrix test succeeded.
EVK-MIMX8ULP
Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the example with with imx-mkimage.(Not running it with your IDE, unless it will be failed to running). Note: After a successful execution, if you need to execute again, you need to completely power down the board and restart it again.
Running the demo
NOTE: Depending on the toolchain configuration, the benchmark result might be different.
BOARD_ReleaseTRDC: 75 start release trdc
BOARD_ReleaseTRDC: 78 finished release trdc, status = 0xd6
BOARD_SetTrdcGlobalConfig: 93 start setup trdc
BOARD_SetTrdcGlobalConfig: 402 finished setup trdc
CMSIS DSP benchmark matrix test start.
arm_mat_add_q15Test: xxx
arm_mat_add_q31Test: xxx
arm_mat_add_f32Test: xxx
arm_mat_sub_q15Test: xxx
arm_mat_sub_q31Test: xxx
arm_mat_sub_f32Test: xxx
arm_mat_mult_q15Test: xxx
arm_mat_mult_q31Test: xxx
arm_mat_mult_f32Test: xxx
arm_mat_inverse_f32Test: xxx
arm_mat_trans_q15Test: xxx
arm_mat_trans_q31Test: xxx
arm_mat_trans_f32Test: xxx
arm_mat_scale_q15Test: xxx
arm_mat_scale_q31Test: xxx
arm_mat_scale_f32Test: xxx
CMSIS DSP benchmark matrix test succeeded.
EVK-MIMXRT595
Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The message about error or success will be output to the terminal.
EVK-MIMXRT685
Hardware requirements
Micro USB cable
EVK-MIMXRT685 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
NOTE: Depending on the toolchain configuration, the benchmark result might be different.
CMSIS DSP benchmark matrix test start.
arm_mat_add_q15Test: xxx
arm_mat_add_q31Test: xxx
arm_mat_add_f32Test: xxx
arm_mat_sub_q15Test: xxx
arm_mat_sub_q31Test: xxx
arm_mat_sub_f32Test: xxx
arm_mat_mult_q15Test: xxx
arm_mat_mult_q31Test: xxx
arm_mat_mult_f32Test: xxx
arm_mat_inverse_f32Test: xxx
arm_mat_trans_q15Test: xxx
arm_mat_trans_q31Test: xxx
arm_mat_trans_f32Test: xxx
arm_mat_scale_q15Test: xxx
arm_mat_scale_q31Test: xxx
arm_mat_scale_f32Test: xxx
CMSIS DSP benchmark matrix test succeeded.
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The message about error or success will be output to the termial.
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The message about error or success will be output to the termial.
FRDM-RW612
Hardware requirements
Micro USB cable
FRDM-RW612 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
The message about error or success will be output to the terminal.
LPCXpresso55S36
Hardware requirements
Mini/micro USB cable
LPCXpresso55s36 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The message about error or success will be output to the termial.
LPCXpresso55S69
Hardware requirements
Mini/micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The message about error or success will be output to the termial.
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The message about error or success will be output to the termial.
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The message about error or success will be output to the termial.
MIMXRT685-AUD-EVK
Hardware requirements
Micro USB cable
MIMXRT685-AUD-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
NOTE: Depending on the toolchain configuration, the benchmark result might be different.
CMSIS DSP benchmark matrix test start.
arm_mat_add_q15Test: xxx
arm_mat_add_q31Test: xxx
arm_mat_add_f32Test: xxx
arm_mat_sub_q15Test: xxx
arm_mat_sub_q31Test: xxx
arm_mat_sub_f32Test: xxx
arm_mat_mult_q15Test: xxx
arm_mat_mult_q31Test: xxx
arm_mat_mult_f32Test: xxx
arm_mat_inverse_f32Test: xxx
arm_mat_trans_q15Test: xxx
arm_mat_trans_q31Test: xxx
arm_mat_trans_f32Test: xxx
arm_mat_scale_q15Test: xxx
arm_mat_scale_q31Test: xxx
arm_mat_scale_f32Test: xxx
CMSIS DSP benchmark matrix test succeeded.
RD-RW612-BGA
Hardware requirements
Micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
The message about error or success will be output to the terminal.