MCUXpresso SDK Documentation

ZPS_tsAplZdpPowerDescStoreRsp

ZPS_tsAplZdpPowerDescStoreRsp#

This structure is used to store Power_Desc_store_rsp message data - a response to a call to the function ZPS_eAplZdpPowerDescStoreRequest(). This response indicates whether the sending node has successfully stored the received Power descriptor in its primary discovery cache.

The ZPS_tsAplZdpPowerDescStoreRspstructure is detailed below.

typedef struct {
        uint8 u8Status;
        uint64 u64IeeeAddr;
        /* Rest of message is variable length */
        ZPS_tsAplZdpNodePowerDescriptor sPowerDescriptor;
} ZPS_tsAplZdpPowerDescStoreRsp;

where:

  • u8Statusis the return status for ZPS_eAplZdpPowerDescStoreRequest().

  • u64IeeeAddris the IEEE/MAC address of the device whose Power descriptor has been stored in the primary discovery cache.

  • sPowerDescriptoris the Power descriptor stored (see Section 9.2.1.1).

Parent topic:ZDP response structures