MCUXpresso SDK Documentation

cau3#

Overview#

The CAU3 Example project is a demonstration program that uses the KSDK software implement several cryptography algorithms using the CAU3 software driver.

Prepare the Demo#

Connect a serial cable from the debug UART port of the board to the PC. Start Tera Term (http://ttssh2.osdn.jp) and make a connection to the virtual serial port.

  1. Start Tera Term

  2. New connection -> Serial

  3. Set apropriate COMx port (x is port number) in Port context menu. Number is provided by operation system and could be different from computer to computer. Select COM number related to virtual serial port. Confirm selected port by OK button.

  4. Set following connection parameters in menu Setup->Serial port… Baud rate: 115200 Data: 8 Parity: none Stop: 1 Flow control: one

  5. Confirm selected parameters by OK button.

Running the demo#

Example output on terminal:

CAU3 Driver Example

AES ECB Test pass SHA-256 Test pass ModMul Test pass

Supported Boards#