MCUXpresso SDK Documentation

usb_pd_source_charger#

Overview#

The PD charger example is a simple demonstration based on the MCUXpresso SDK PD stack.
The application simulate charger product.
The demo only works as source and is external powered.

System Requirement#

Hardware requirements#

  • One or two Type-C shield board

  • One or two 9V DC power suppliers

  • Type-C Cable

  • One or two hardwares (Tower module/base board, and so on) for a specific device, for example: lpcxpresso54114 board

  • Personal Computer

Software requirements#

  • The project files are in:
    <MCUXpresso_SDK_Install>/boards//usb_examples/usb_pd_source_charger//.

The is Bare Metal or FreeRTOS OS.

  • Terminal tool.

Getting Started#

Hardware Settings#


For detailed instructions, see the appropriate board User’s Guide.

Set the hardware jumpers (Tower system/base module) to default settings.

Prepare the example#

  1. Download the program to the target board.

  2. Power on Type-C shield board then power on development board.

Run the example#

  1. Connect the OpenSDA USB port to the PC and open terminal.

  2. This charger provide power 5V/2.7A and 9V/1.5A.

  3. Connect the sink with Type-C cable to the board, The board will print the sink’s request power information.
    For example: Download usb_pd_charger_battery or usb_pd_sink_battery demo to another board and connect to the tested board.

Supported Boards#

  • MIMXRT1170-EVKB

  • FRDM-K22F

  • LPCXpresso55S69

  • EVK-MIMXRT1064

  • MIMXRT685-AUD-EVK

  • LPCXpresso55S16

  • MIMXRT1060-EVKB

  • MIMXRT1040-EVK

  • FRDM-MCXN947

  • FRDM-MCXN947T

  • MIMXRT1024-EVK

  • LPCXpresso55S28

  • LPCXpresso55S36

  • MCX-N5XX-EVK

  • MIMXRT1060-EVKC

  • MIMXRT1160-EVK

  • MIMXRT1180-EVK

  • FRDM-K32L2A4S

  • EVK-MIMXRT1020

  • MIMXRT700-EVK

  • FRDM-IMXRT700

  • EVK-MIMXRT595

  • EVK-MIMXRT685

  • MCX-N9XX-EVK

  • EVKB-IMXRT1050

  • EVK-MIMXRT1015

  • FRDM-MCXN236

  • FRDM-IMXRT1152