pflash_swap#
Overview#
The flash_swap example shows how to use flash swap feature:
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
PFLASH Swap example Start PFlash Information: Total Program Flash Size: xx KB, Hex: (xx) Total Program Flash Block Count: xx Program Flash Sector Size: xx KB, hex: (xx) Flash is xx Original swap indicator address: xx Current swap system status: xx Validating the backup example image… Backup example image is invalid Start to program backup example image Finish programming backup example image Checking the system status… It is first swap for the system Start to erase test data on lower pflash before swapping system Finish erasing test data Start to program backup test data on upper pflash Finish programming backup test data Start to swap the system
Perform a system reset
FLASH Swap example Start PFlash Information: Total Program Flash Size: xx KB, Hex: (xx) Total Program Flash Block Count: xx Program Flash Sector Size: xx KB, hex: (xx) Flash is xx Original swap indicator address: xx Current swap system status: xx Validating the backup example image… Backup example image is valid Checking the system status… The system has been swapped successfully Start to erase test data on lower pflash before exiting this example Finish erasing test data
End of PFLASH Swap example
Supported Boards#
FRDM-KE17Z512
Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
These instructions are displayed/shown on the terminal window:
PFLASH Swap example Start
PFlash Information:
Total Program Flash Size: xx KB, Hex: (xx)
Total Program Flash Block Count: xx
Program Flash Sector Size: xx KB, hex: (xx)
Flash is xx
Original swap indicator address: xx
Current swap system status: xx
Validating the backup example image...
Backup example image is invalid
Start to program backup example image
Finish programming backup example image
Checking the system status...
It is first swap for the system
Start to erase test data on lower pflash before swapping system
Finish erasing test data
Start to program backup test data on upper pflash
Finish programming backup test data
Start to swap the system
Perform a system reset
FLASH Swap example Start
PFlash Information:
Total Program Flash Size: xx KB, Hex: (xx)
Total Program Flash Block Count: xx
Program Flash Sector Size: xx KB, hex: (xx)
Flash is xx
Original swap indicator address: xx
Current swap system status: xx
Validating the backup example image...
Backup example image is valid
Checking the system status...
The system has been swapped successfully
Start to erase test data on lower pflash before exiting this example
Finish erasing test data
End of PFLASH Swap example