MCUXpresso SDK Documentation

dac_continuous_lptmr_edma

dac_continuous_lptmr_edma#

Overview#

The demo shows how to use the LPTMR to generate a DAC trigger and use the DMA to transfer data into DAC buffer.

In this example, DAC is first set to normal buffer mode. LPTMR is as DAC hardware trigger source and DMA would work when DAC read pointer is zero. When run the example, the DAC is triggered by LPTMR and the read pointer increases by one, every time the trigger occurs. When the read pointer reaches the upper limit, it goes to zero directly in the next trigger event. While read pointer goes to zero, DMA request will be triggered and transfer data into DAC buffer. The user should probe the DAC output with a oscilloscope to see the Half-sine signal.

Supported Boards#

FRDM-K32L2A4S
Hardware requirements
  • Mini/Micro USB cable

  • FRDM-K32L2A4S board

  • Voltmeter

  • Personal Computer

Board settings

To measure the DAC output, connect J4-11 to positive of Voltmeter

Prepare the Demo
  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

  5. A multimeter may be used to measure the DAC output voltage.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

DAC CONTINUOUS LPTMR EDMA DEMO
Please probe the DAC output with a oscilloscope.

Then user can measure the DAC output pin to check responding voltage.