MCUXpresso SDK Documentation

cadc_parallel_independent_conversion

cadc_parallel_independent_conversion#

Overview#

The cadc_parallel_independent_conversion example shows how to use each converter independently.

In this example, the CADC is configured as “kCADC_ScanModeTriggeredParallelIndependent” work mode. User should indicate 4 channel pairs to provide the differential voltage signal (can be controlled by user) as the inputs for CADC sample slots. These sample slots would be assembled into the two short conversion sequences (can include 8 sample slots as most). Also the “simultaneous mode” is disabled, so that each converter can be operated by their own control logic separately.

When running the project, typing any key into debug console would trigger the conversion. And then, the conversion result data of the converter A’s sample slots (Sample 0, 1) would be displayed in the terminal. Type the keyboard again to trigger the converter B, the conversion result data of the converter B’s two sample slots (Sample 8, 9) would be displayed.

Supported Boards#

MC56F80000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F80000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2

  2. Reset pin setting:

    Connect J11 pin2 and pin3

  3. Debugger setting:

    Connect J13 pin 1-2, 3-4, 5-6, 7-8

Board settings
  • Supply external voltage(0~3.3V) to ANA4(J4-4) and ANA5(J4-6).

  • Supply external voltage(0~3.3V) to ANB4(J4-10) and ANB5(J4-12).

  • Supply external voltage(0~3.3V) to ANB2(J2-9) and ANB3(J2-5).

Note: The sample0 works in fully differential mode and the differential pair is selected as ANA4 and ANA5. The sample1 works in fully differential mode and the differential pair is selected as ANA6 and ANA7. And the thermistor in MC56F80000-EVK board is connected to ANA6 and ANA7. The sample8 works in fully differential mode and the differential pair is selected as ANB4 and ANB5. The sample9 works in fully differential mode and the differential pair is selected as ANB2 and ANB3.

Prepare the Demo
  1. Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with Multilink debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

CADC parallel independent conversion example.
Press any key to trigger the conversion ...

Sample 0        Sample 1        Sample 8        Sample 9

16344           23760           28752           28304
16344           23760           28752           28352

................
................

User can press any key to continue the converter and get more converter data. Touching thermistor on board then the output values of sample will be updated.

MC56F81000-EVK
Hardware requirements
  • 2 x Micro USB cable

  • MC56F81000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J8 pin2 and pin3 Connect J5 pin1 and pin2 Connect J6 pin1 and pin2

  2. Onboard PnE U-MultiLink debugger setting:

    Connet J11 pin2 and pin3 Connect J13 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger PnE U-MultiLink. Note: when use external debugger(connected to J10), leave all J13 pins open.

Board settings
  • Supply external voltage(0~3.3V) to ANA4(J4-4) and ANA5(J4-6).

  • Supply external voltage(0~3.3V) to ANB4(J4-10) and ANB5(J4-12).

  • Supply external voltage(0~3.3V) to ANB2(J2-9) and ANB3(J2-5).

Note: The sample0 works in fully differential mode and the differential pair is selected as ANA4 and ANA5. The sample1 works in fully differential mode and the differential pair is selected as ANA6 and ANA7. And the thermistor in MC56F81000-EVK board is connected to ANA6 and ANA7. The sample8 works in fully differential mode and the differential pair is selected as ANB4 and ANB5. The sample9 works in fully differential mode and the differential pair is selected as ANB2 and ANB3.

Prepare the Demo
  1. Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.

  2. Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board with PnE U-MultiLink debug configuration.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted default FCF(flash configuration field) makes the MCU boot from flash.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

CADC parallel independent conversion example.
Press any key to trigger the conversion ...

Sample 0        Sample 1        Sample 8        Sample 9

16344           23760           28752           28304
16344           23760           28752           28352

................
................

User can press any key to continue the converter and get more converter data. Touching thermistor on board then the output values of sample will be updated.

MC56F83000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F83000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J19 pin2 and pin3 Connect J12 pin1 and pin2 Connect J13 pin1 and pin2 Connect J15 pin1 and pin2 Connect J16 pin2 and pin3 Connect J17 pin1 and pin2

  2. Onboard OSJTAG debugger setting:

    Leave J5 open Leave J6 open Note: J6 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J11 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J10), leave all J11 pins open.

Board settings
  • Supply external voltage(0~3.3V) to ANA4(J4-4) and ANA5(J4-6).

  • Supply external voltage(0~3.3V) to ANB0(J2-3) and ANB1(J4-8).

  • Supply external voltage(0~3.3V) to ANB2(J2-9) and ANB3(J2-5).

Note: The sample0 works in fully differential mode and the differential pair is selected as ANA4 and ANA5. The sample1 works in fully differential mode and the differential pair is selected as ANA6 and ANA7. And the thermistor in MC56F83000-EVK board is connected to ANA6 and ANA7. The sample8 works in fully differential mode and the differential pair is selected as ANB0 and ANB1. The sample9 works in fully differential mode and the differential pair is selected as ANB2 and ANB3.

Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J8) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted that default FCF(flash configuration field) setting makes MCU boot from bootloader. So after reset button press, it will wait 5s(wait in bootloader) to run the application code.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

CADC parallel independent conversion example.
Press any key to trigger the conversion ...

Sample 0        Sample 1        Sample 8        Sample 9

16344           23760           28752           28304
16344           23760           28752           28352

................
................

User can press any key to continue the converter and get more converter data. Touching thermistor on board then the output values of sample will be updated.

TWR-MC56F8200
Hardware requirements
  • Mini USB cable

  • TWR-MC56F8200 board

  • Personal Computer

Board hardware common setting
  1. HW reworkd(workaround):

    Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.

  2. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  3. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  4. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings

Connect J23 with jumper, 1-2, 3-4. Connect J19 with jumper, 1-2, 3-4. Connect J1 with jumper, 1-2, 3-4. Connect J2 with jumper, 1-2, 3-4.

Note: The sample0(thermistor 4) works in fully differential mode and the differential pair is selected as ANA4 and ANA5. The sample1(thermistor 3) works in fully differential mode and the differential pair is selected as ANA6 and ANA7. The sample8(thermistor 1) works in fully differential mode and the differential pair is selected as ANB4 and ANB5. The sample9(thermistor 2) works in fully differential mode and the differential pair is selected as ANB6 and ANB7.

Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

CADC parallel independent conversion example.
Press any key to trigger the conversion ...

Sample 0        Sample 1        Sample 8        Sample 9

25736           18200           16992           25640
25656           18192           16992           25640
................
................

User can press any key to continue the converter and get more converter data. Touching thermistor on board then the output values of sample will be updated.

TWR-MC56F8400
Hardware requirements
  • Mini USB cable

  • TWR-MC56F8400 board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  2. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  3. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings

Connect J23 with jumper, 1-2, 3-4. Connect J19 with jumper, 1-2, 3-4. Connect J1 with jumper, 1-2, 3-4. Connect J2 with jumper, 1-2, 3-4.

Note: The sample0(thermistor 4) works in fully differential mode and the differential pair is selected as ANA4 and ANA5. The sample1(thermistor 3) works in fully differential mode and the differential pair is selected as ANA6 and ANA7. The sample8(thermistor 1) works in fully differential mode and the differential pair is selected as ANB4 and ANB5. The sample9(thermistor 2) works in fully differential mode and the differential pair is selected as ANB6 and ANB7.

Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

CADC parallel independent conversion example.
Press any key to trigger the conversion ...

Sample 0        Sample 1        Sample 8        Sample 9

25736           18200           16992           25640
25656           18192           16992           25640
................
................

User can press any key to continue the converter and get more converter data. Touching thermistor on board then the output values of sample will be updated.