MCUXpresso SDK Documentation

lwip_dhcp_usb_freertos#

Overview#

The lwip_dhcp demo application demonstrates a DHCP and ping demo on the lwIP TCP/IP and USB stack. The application acts as a DHCP client and prints the status as it is progressing. Once the interface is being bound to an IP address obtained from DHCP server, address information is printed. The application will get ip adress www.nxp.com and ping the ip address.

Prepare the Demo#

  1. Connect a USB cable between the PC host and the OpenSDA(or USB to Serial) USB port on the target board.

  2. Open a serial terminal on PC for OpenSDA serial(or USB to Serial) device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

refer to MCUXpresso SDK USB RNDIS & LWIP User Guide

Supported Boards#

EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

No special settings are required.

MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

Board settings

No special settings are required.

MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

No special settings are required.

MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings

No special settings are required.

EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1020 board

  • Personal Computer

Board settings

No special settings are required.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

Board settings

No special settings are required.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.

MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

Board settings

No special settings are required.

MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

Board settings

No special settings are required.

MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings

No special settings are required.

FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings

No special settings are required.

FRDM-MCXN947T
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947T board

  • Personal Computer

Board settings

No special settings are required.

FRDM-RW612
Hardware requirements
  • USB-C cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

No special settings are required.

LPCXpresso54628
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings
  • The Jumper settings: J9 1-2 high speed mode,2-3 full speed mode; J10 open high speed, shunt full speed; J11 2-3, J12 2-3, J13 2-3 , need provide external power through J1.

LPCXpresso54S018
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso54s018 board

  • Personal Computer

Board settings
  • The Jumper settings: J9 1-2 high speed mode,2-3 full speed mode; J10 open high speed, shunt full speed; J11 2-3, J12 2-3, J13 2-3 , need provide external power through J1.

MCX-N5XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

Board settings

No special settings are required.

MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings

No special settings are required.

RD-RW612-BGA
Hardware requirements
  • Mini/micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings

No special settings are required.

FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings

No special settings are required.

FRDM-MCXA577
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA577 board

  • Personal Computer

Board settings

No special settings are required.