MCUXpresso SDK Documentation

ZPS_tsAplZdpMgmtRtgRsp

ZPS_tsAplZdpMgmtRtgRsp#

This structure is used to store Mgmt_Rtg_rsp message data - a response to a call to the function ZPS_eAplZdpMgmtRtgRequest(). This response reports the contents of the remote node’s Routing table

The ZPS_tsAplZdpMgmtRtgRspstructure is detailed below.

typedef struct {
    uint8 u8Status;
    uint8 u8RoutingTableEntries;
    uint8 u8StartIndex;
    uint8 u8RoutingTableCount;
    /* Rest of the message is variable length */
    ZPS_tsAplZdpRtEntry* pRoutingTableList;
} ZPS_tsAplZdpMgmtRtgRsp;

where:

  • u8Statusis the return status for ZPS_eAplZdpMgmtRtgRequest()

  • u8RoutingTableEntriesis the total number of Routing table entries on the remote node

  • u8StartIndexis the Routing table index of the first entry reported in this response (through pRoutingTableList)

  • u8RoutingTableCountis the number of Routing table entries reported in this response (through pRoutingTableList)

  • pRoutingTableListis a pointer to the first entry in the list of reported Routing table entries. Each entry is of the type ZPS_tsAplZdpRtEntrydetailed below

    
    typedef struct
    {
        uint16 u16NwkDstAddr; /**< Destination Network address */
        uint16 u16NwkNxtHopAddr; /**< Next hop Network address */
      union
        {
        struct
           {
            unsigned u3Status:3;
            unsigned u1MemConst:1;
            unsigned u1ManyToOne:1;
            unsigned u1RouteRecordReqd:1;
            unsigned u1Reserved:2;
            } bfBitfields;
            uint8 u8Field;
      } uAncAttrs;
    } ZPS_tsAplZdpRtEntry;
    

    where:

    • u16NwkDstAddris the destination network address of the route.

    • u16NwkNxtHopAddris the ‘next hop’ network address of the route.

    • u3Status:3is the 3-bit status for the route:

      • 000 = ACTIVE

      • 001 = DISCOVERY_UNDERWAY

      • 010 = DISCOVERY_FAILED

      • 011 = INACTIVE

      • 100 = VALIDATION_UNDERWAY

      • 101-111 = Reserved.

    • u1MemConst:1is a bit indicating whether the device is a memory-constrained concentrator.

    • u1ManyToOne:1is a bit indicating whether the destination node is a concentrator that issued a many-to-one request.

    • u1RouteRecordReqd:1is a bit indicating whether a route record command frame. should be sent to the destination before the next data packet.

    • u1Reserved:2are reserved bits.

    • u8Fieldcontains the full set of flags of the bfBitfieldssub-structure, with u3Status:3occupying the most significant bits and u1Reserved:2occupying the least significant bits (for a big-endian device).

Parent topic:ZDP response structures