ZPS_tsAplZdpRemoveBkupBindEntryReq
This structure is used by the ZPS_eAplZdpRemoveBkupBindEntryRequest() function. It represents a request to a remote node to remove the back-up of an entry from the local primary binding table cache.
The ZPS_tsAplZdpRemoveBkupBindEntryReqstructure is detailed below.
typedef struct {
uint64 u64SrcAddress;
uint8 u8SrcEndPoint;
uint16 u16ClusterId;
uint8 u8DstAddrMode;
union {
struct {
uint16 u16DstAddress;
} sShort;
struct
{
uint64 u64DstAddress;
uint8 u8DstEndPoint;
} sExtended;
};
} ZPS_tsAplZdpRemoveBkupBindEntryReq;
where:
u64SrcAddressis the IEEE address of the source node for the binding entry.u8SrcEndpointis the number of the source endpoint for the binding (1-240).u16ClusterIdis the ID of the cluster (on the local endpoint) for the binding.u8DstAddrModeis the destination addressing mode for remaining elements (see the Table below) .u16DstAddressis the address the destination node for the binding (address type according to setting ofu8DstAddrMode).u8DstEndPointis the number of the destination endpoint for the binding (1-240).
Addressing modes
u8DstAddrMode |
Code |
Description |
|---|---|---|
0x01 |
ZPS_E_ADDR_MODE_GROUP |
16-bit Group address |
0x03 |
ZPS_E_ADDR_MODE_IEEE |
64-bit IEEE/MAC address |
Parent topic:ZDP Request structures