se05x_cloud_aws#
Overview#
This demo demonstrates connection to AWS IoT Console using pre-provisioned device credentials and publish/subscribe procedure using MQTT.
Supported Boards#
LPCXpresso55S69
Hardware requirements
Mini/micro USB cable
LPCXpresso55s69 board
Personal Computer
CMWC1ZZABR-107-EVB by muRata
OM- SE050ARD or OM- SE051ARD
Board settings
Jumper settings for OM- SE050ARD & OM- SE051ARD: -J14 3-4 (Default): EdgeLock SE05x_VCC pin routed to SE05X_VOUT pin -J15 3-4 (Default): I2C target SDA connection -J17 3-4 (Default): I2C target SCL connection
Prerequisites
Active AWS account
The Plug & Trust MW package can be downloaded from https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-and-trust-secure-element-family-enhanced-iot-security-with-high-flexibility:SE050#design-resources
Any Serial communicator
Flash VCOM binary on the device at flash address 0x00000000. VCOM binary se05x_vcom-T1oI2C-
.bin can found in Plug & Trust MW package :simw-top\binaries\MCU folder.
Creating and updating device keys and certificates to SE
Check the vcom port number
Go to the EdgeLock SE05x Plug & Trust middleware ..\simw-top\binaries\PCWindows\ssscli folder and call:
Provision_AWS.exe
note: is detected vcom port Certificates and Keys are generated at
simw-top/binaries/PCWindows/ssscli/aws
Creating a device on AWS account
Refer - https://docs.aws.amazon.com/iot/latest/developerguide/iot-gs-first-thing.html
Running the Demo
In the ‘
\source\aws_iot_config.h’ file, update the endpoint in the macro “clientcredentialMQTT_BROKER_ENDPOINT” Connect your board to open network on wifi.
Update
clientcredentialWIFI_SSIDandclientcredentialWIFI_PASSWORDin<PROJECT>\se_hostlib\demos\ksdk\common\wifi_config.hwith your wifi credentials.Build the project and flash the binary on board.
The log below shows the output of the demo in the terminal window. The log can be different based on your local network configuration. App :INFO :PlugAndTrust_v04.04.00_20230811 sss :INFO :atr (Len=35) 01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00 01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31 00 00 00 sss :WARN :Communication channel is Plain. sss :WARN :!!!Not recommended for production use.!!! App :INFO :AWS subscribe publish example
App :INFO :Turning WIFI ON App :INFO :Connecting to network:iot_wifi_ssid App :INFO :Wi-Fi is connecting…
App :INFO :Wi-Fi is connecting…
App :INFO :Wi-Fi is connecting…
App :INFO :Wi-Fi is connecting…
App :INFO :Wi-Fi is connected to: iot_wifi_ssid, IP Address: 192.168.0.106 [INFO] Create a TCP connection to a29rg0ytflhg6y.iot.eu-central-1.amazonaws.com: 8883. [INFO] (Network connection 0x20208970) TLS handshake successful. [INFO] (Network connection 0x20208970) Connection to a29rg0ytflhg6y.iot.eu-centr al-1.amazonaws.com [INFO] MQTT connection established with the broker. [INFO] MQTT connection successfully established with broker.
[INFO] A clean MQTT connection is established. Cleaning up all the stored outgoing publishes.
App :INFO :MQTT Connection successfully established [INFO] Attempt to subscribe to the MQTT topic $aws/things/K64f_1/shadow/update/accepted. App :INFO :MQTT Subscribed [INFO] the published payload:{“msg” : “hello from SDK QOS0 : 0”}
[INFO] PUBLISH sent for topic sdkTest/sub to broker with packet ID 2.
App :INFO :Published message {“msg” : “hello from SDK QOS0 : 0”} App :INFO :AWS demo passed App :INFO :Demo Example Finished