tmu_monitor_report#
Overview#
The TMU example shows how to configure TMU register to monitor and report the temperature from one or more remote temperature measurement sites located on the chip.
TMU has access to multiple temperature measurement sites strategically located on the chip. It monitors these sites and can signal an alarm if a programmed threshold is ever exceeded.
Note: Before monitoring the temperature, we must programming the calibration table.
Supported Boards#
EVK-MIMX8MQ
Hardware requirements
Micro USB cable
MIMX8MQ6-EVK board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW701 to power on the board
Connect a USB cable between the host PC and the J1701 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
TMU monitor report example.
site 1 immediate temperature is too high. 41°C
site 1 immediate temperature is too high. 41°C
site 0 immediate temperature is too high. 41°C
site 1 immediate temperature is too high. 42°C
site 0 immediate temperature is too high. 41°C
site 1 immediate temperature is too high. 42°C
...