MCUXpresso SDK Documentation

scg

scg#

Overview#

The SCG example shows how to use SCG driver:

  1. How to setup the SCG clock source.

  2. How to use SCG clock while power mode switch.

  3. How to use SCG APIs to get clock frequency.

This example prints the clock frequency through the terminal using the SDK driver.

Supported Boards#

FRDM-K32L2A4S
Hardware requirements
  • Mini USB cable

  • FRDM-K32L2A4S board

  • Personal Computer

Board settings

This demo prints through the OpenSDA serial port, don’t need special board setting.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port (J13) on frdmk32l2a4s board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. For detailed instructions, see Getting Started with Software Development Kit for K32L2A (document SDKK32L2AGSUG).

Running the demo

When the demo runs successfully, will get the following messages on the OpenSDA terminal.

SCG Example Start

SCG clock source frequency
SIRC clock: 8000000 Hz
FIRC clock: 48000000 Hz
SPLL clock: 72000000 Hz

Current power mode: VLPR
Core clock: 4000000 Hz
Slow clock: 1000000 Hz

Current system clock: RUN
Core clock: 48000000 Hz
Slow clock: 24000000 Hz

Current power mode: HSRUN
Core clock: 72000000 Hz
Slow clock: 24000000 Hz

Current power mode: RUN
Core clock: 8000000 Hz
Slow clock: 4000000 Hz

SCG Example End.
FRDM-KE15Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE15Z board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

SCG Example Start



SCG clock source frequency

SIRC clock: 8000000 Hz

FIRC clock: 48000000 Hz

LPFLL clock: 48000000 Hz



Current power mode: VLPR

Core clock: 4000000 Hz

Slow clock: 1000000 Hz




Current system clock: RUN

Core clock: 48000000 Hz

Slow clock: 24000000 Hz




Current power mode: RUN

Core clock: 8000000 Hz

Slow clock: 4000000 Hz




SCG Example End.
FRDM-KE16Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE16Z board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

SCG Example Start

SCG clock source frequency
SIRC clock: 8000000 Hz
FIRC clock: 48000000 Hz
LPFLL clock: 48000000 Hz

Current power mode: VLPR
Core clock: 4000000 Hz
Slow clock: 1000000 Hz

Current system clock: RUN
Core clock: 48000000 Hz
Slow clock: 24000000 Hz

Current power mode: RUN
Core clock: 8000000 Hz
Slow clock: 4000000 Hz

SCG Example End.
FRDM-KE17Z
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

SCG Example Start



SCG clock source frequency

SIRC clock: 8000000 Hz

FIRC clock: 48000000 Hz

LPFLL clock: 48000000 Hz



Current power mode: VLPR

Core clock: 4000000 Hz

Slow clock: 1000000 Hz




Current system clock: RUN

Core clock: 48000000 Hz

Slow clock: 24000000 Hz




Current power mode: RUN

Core clock: 8000000 Hz

Slow clock: 4000000 Hz




SCG Example End.
FRDM-KE17Z512
Hardware requirements
  • Micro USB cable

  • FRDM-KE17Z512 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

SCG Example Start



SCG clock source frequency

SIRC clock: 8000000 Hz

FIRC clock: 48000000 Hz

LPFLL clock: 48000000 Hz



Current power mode: VLPR

Core clock: 4000000 Hz

Slow clock: 1000000 Hz




Current system clock: RUN

Core clock: 48000000 Hz

Slow clock: 24000000 Hz




Current power mode: RUN

Core clock: 8000000 Hz

Slow clock: 4000000 Hz




SCG Example End.
FRDM-MCXE247
Hardware requirements
  • USB-C cable

  • FRDM-MCXE247 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

SCG Example Start

SCG clock source frequency
SIRC clock: 8000000 Hz
FIRC clock: 48000000 Hz
SPLL clock: 72000000 Hz

Current power mode: VLPR
Core clock: 4000000 Hz
Slow clock: 1000000 Hz
Bus clock: 4000000 Hz

Current system clock: RUN
Core clock: 48000000 Hz
Slow clock: 24000000 Hz
Bus clock: 48000000 Hz

Current power mode: HSRUN
Core clock: 72000000 Hz
Slow clock: 24000000 Hz
Bus clock: 72000000 Hz

Current power mode: RUN
Core clock: 8000000 Hz
Slow clock: 4000000 Hz
Bus clock: 8000000 Hz

SCG Example End.