psa_crypto_examples_thread#
Overview#
The mbedTLS PSA Crypto example thread program performs PSA API testing within Multi threaded environment and prints results to the terminal.
Supported Boards#
FRDM-RW612
Hardware requirements
Mini/micro USB cable
FRDM-RW612 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the terminal will display similar information like the following:
Mbedtls - PSA - Crypto - examples - Multithread
============================ Create thread one successfully Create thread two successfully Thread 1 is running… Thread 1 is running… Thread 2 is running… Thread 1 is running… Thread 1 is running… Thread 1 is running… Thread 2 is running… Thread 1 is running… Thread 1 is running… Thread 2 is running… Thread 1 is running… Thread 1 is running… Thread 1 is running… Thread 2 is running…
RD-RW612-BGA
Hardware requirements
Mini/micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the terminal will display similar information like the following:
Mbedtls - PSA - Crypto - examples - Multithread
============================ Create thread one successfully Create thread two successfully Thread 1 is running… Thread 1 is running… Thread 2 is running… Thread 1 is running… Thread 1 is running… Thread 1 is running… Thread 2 is running… Thread 1 is running… Thread 1 is running… Thread 2 is running… Thread 1 is running… Thread 1 is running… Thread 1 is running… Thread 2 is running…