mcxromapi_mem_interface#
Hardware requirements#
Mini/micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
Internal flash example start:
Calling API_Version!
IAP API version = x.x.x
Calling API_Init!
API_Init Successfully!
PFlash Information:
Program Flash Base Address: xx
Total Program Flash Size: xx
Program Flash Sector Size: xx
Erasing internal flash
Successfully erased internal flash xx -> xx
Calling MEM_Write to program internal flash!
Successfully Programmed and Verified Location xx -> xx
End of internal flash example!
Supported Boards#
FRDM-MCXN236
Hardware requirements
Type-C USB cable
FRDM-MCXN236 board
Personal Computer
Board settings
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J10) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Internal flash example start:
Calling API_Version!
IAP API version = x.x.x
Calling API_Init!
API_Init Successfully!
PFlash Information:
Program Flash Base Address: xx
Total Program Flash Size: xx
Program Flash Sector Size: xx
Erasing internal flash
Successfully erased internal flash xx -> xx
Calling MEM_Write to program internal flash!
Successfully Programmed and Verified Location xx -> xx
End of internal flash example!
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Internal flash example start:
Calling API_Version!
IAP API version = x.x.x
Calling API_Init!
API_Init Successfully!
PFlash Information:
Program Flash Base Address: xx
Total Program Flash Size: xx
Program Flash Sector Size: xx
Erasing internal flash
Successfully erased internal flash xx -> xx
Calling MEM_Write to program internal flash!
Successfully Programmed and Verified Location xx -> xx
End of internal flash example!
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
Board settings
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Internal flash example start:
Calling API_Version!
IAP API version = x.x.x
Calling API_Init!
API_Init Successfully!
PFlash Information:
Program Flash Base Address: xx
Total Program Flash Size: xx
Program Flash Sector Size: xx
Erasing internal flash
Successfully erased internal flash xx -> xx
Calling MEM_Write to program internal flash!
Successfully Programmed and Verified Location xx -> xx
End of internal flash example!
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Internal flash example start:
Calling API_Version!
IAP API version = x.x.x
Calling API_Init!
API_Init Successfully!
PFlash Information:
Program Flash Base Address: xx
Total Program Flash Size: xx
Program Flash Sector Size: xx
Erasing internal flash
Successfully erased internal flash xx -> xx
Calling MEM_Write to program internal flash!
Successfully Programmed and Verified Location xx -> xx
End of internal flash example!
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Internal flash example start:
Calling API_Version!
IAP API version = x.x.x
Calling API_Init!
API_Init Successfully!
PFlash Information:
Program Flash Base Address: xx
Total Program Flash Size: xx
Program Flash Sector Size: xx
Erasing internal flash
Successfully erased internal flash xx -> xx
Calling MEM_Write to program internal flash!
Successfully Programmed and Verified Location xx -> xx
End of internal flash example!