MCUXpresso SDK Documentation

lwip_mqtt_enet_qos_freertos

lwip_mqtt_enet_qos_freertos#

Overview#

The lwip_mqtt demo application demonstrates MQTT client connecting to MQTT broker via unsecured socket. The application obtains IP and DNS addresses from DHCP and resolves broker’s hostname if needed. Then it connects to the broker and subscribes to the “lwip_topic/#” and “lwip_other/#” topics. Further it publishes five messages to the “lwip_topic/100” which are also received back as the board is subscribed to the “lwip_topic/#”. It then disconnects from the broker.

Supported Boards#