kbi#
Overview#
The KBI Example project is a demonstration program that uses the KSDK software to use keyboard interrupt. The example uses one KBI pin to generate a raising edge interrupt to show the example.
Supported Boards#
FRDM-KE02Z40M
Hardware requirements
Mini USB cable
Two FRDM-KE02Z boards
Personal Computer
Board settings
connect 2# & 6# on J2.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
KBI Driver Example Start.
The KBI keyboard interrupt has happened!
KBI Driver Example End.