ZPS_tsAplZdpNodeDescRsp#
This structure is used to store Node_Desc_rsp message data - a response to a call to the function ZPS_eAplZdpNodeDescRequest(). This response contains the Node descriptor of the node with a given network address.
The ZPS_tsAplZdpNodeDescRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint16 u16NwkAddrOfInterest;
/* Rest of the message is variable length */
ZPS_tsAplZdpNodeDescriptor tsNodeDescriptor;
} ZPS_tsAplZdpNodeDescRsp;
where:
u8Statusis the return status for ZPS_eAplZdpNodeDescRequest().u16NwkAddrOfInterestis the network address of the remote node that sent the response (this is the network address that was specified in the request).tsNodeDescriptoris the returned Node descriptor, a structure of typeZPS_tsAplZdpNodeDescriptor(detailed in Section 9.2.1.1). This is only included ifu8Statusreports success.
Parent topic:ZDP response structures