tdet#
Overview#
The TDET Example project is a demonstration program that uses the MCUX SDK software to set up Digital Tamper (TDET) peripherial. Then tests the expected behaviour.
Running the demo#
When the demo runs successfully, the terminal displays similar information like the following:
TDET Peripheral Driver Example
Tampering detected Tamper Detect Flag is set
Passive tamper example
No tampering detected on PIN0
Active tamper example
No tampering detected on active tamper
End of example