niobe4analog_flexspi_nor#
Overview#
The FLASIAP NOR project is a simple demonstration program of the SDK FLASIAP NOR driver. It erases and programs a portion of external Nor flash connected with FLEXSPI. Some simple flash command willbe executed,such as Write Enable, Erase sector, Program page. Example will first erase the sector and program a page into the flash, at last check if the data in flash is correct.
Supported Boards#
LPCXpresso55S36
Hardware requirements
Mini/micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
Connect pin 1-2 of JP41,JP42,JP43,JP44,JP45,JP64 and JP65. Close JP66,JP67,JP68 and JP69.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
FLEXSPI NOR example started!
Successfully get FLEXSPI NOR configuration block
Successfully init FLEXSPI serial NOR flash
Serial NOR flash Information:
Serial NOR flash size: xx KB, Hex: (xx)
Serial NOR flash sector size: xx KB, Hex: (xx)
Serial NOR flash page size: xx B, Hex: (xx)
Erasing serial NOR flash over FLEXSPI
Successfully erased one sector of NOR flash device xx -> xx
Program a buffer to a page of NOR flash
Access serial NOR flash over AHB
Successfully programmed and verified location FLEXSPI AMBA memory xx -> xx
End of FLEXSPI NOR Example!