MCUXpresso SDK Release Notes#
Development tools#
The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.
SDK 25.12.00 is the final release that includes MCUXpresso IDE support for MCX W7x devices. Beginning with SDK 26.x.x, MCUXpresso IDE will no longer be supported for MCX W7x development, and MCUXpresso for Visual Studio Code will become the recommended integrated development environment.
IAR Embedded Workbench for Arm, version is 9.70.4
MCUXpresso for VS Code v26.06
GCC Arm Embedded Toolchain 14.2.x
Supported development systems#
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
|---|---|
MCXW72-LOC |
MCXW727CMFTA |
MCUXpresso SDK release package#
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support#
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support#
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples#
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS#
FreeRTOS#
Real-time operating system for microcontrollers from Amazon
Middleware#
GenFSK link layer#
The Generic FSK protocol enables radio operation using a custom GFSK/GMSK or MSK modulation format.
Main Features supported:
Highly configurable packet structure
Optimized Sequence Command Set
High-precision timebase to maintain network timing
Two timer-compare mechanisms for Interrupt Generation and Sequence Launching
Hardware automation for packet transmit and receive, CRC and Whitening
Up to four network addresses to synchronize to, can be 8-bit, 16-bit or 32-bit
Packet Lengths up to 2047 Bytes
Support complex auto-sequence, like CCA before TX, Auto-ACK, TR.
Many operating modes can support the sending and receiving of multiple protocol packets, such as Bluetooth LE.
Wireless XCVR#
The XCVR component provides a base Transceiver Driver for the 2.4 GHz narrowband radio.
Bluetooth LE Controller#
Main features supported:
Peripheral Role
Central Role
Multiple PHYs (1 Mbps, 2 Mbps, Coded PHY)
Asymmetric Connections
Public/Random/Static Addresses
Network/Device Privacy Modes
Extended Advertising
Extended Scanning
Passive/Active Scanning
LE Encryption
LE Ping Procedure
HCI Test Interface
UART Test Interface
Randomized Advertising Channel Indexing
Sleep Clock Accuracy Update - Mechanism
ADI Field in Scan Response Data
HCI Support for Debug Keys in LE - Secure Connections
Main capabilities supported:
Simultaneous scanning 1 Mbps and Long Range
Scanning and advertising in parallel
24 connections as a central role
24 connections as a peripheral role
Any combination of central and peripheral roles (24 connections maximum)
8 connections with a 7.5 ms connection interval
Five advertising sets in parallel.
26 Accept List entries
36 Resolvable Private Address (RPA) entries
Up to two Chain Packets per Extended Advertising set
Enhanced Notification on end of - Scanning/Advertising/Connection events
Connection event counters associated to Bluetooth LE packet reception
Timestamp associated to Bluetooth LE packet reception
RF channel info associated to Bluetooth LE packet reception
NXP proprietary Bluetooth LE Handover feature
Decision Based Advertising Filtering (DBAF)
Advertising Coding Selection (ACS)
Periodic Advertising with Responses (PAwR) Additional features supported for KW47 and MCX W72 devices:
Channel Sounding Additional features supported as EAR (\Early Access Release) in the KW47 experimental build:
Inline PCT Transfer (IPT)
RTT_PHY capability
Channel Sounding Enhancement 1
Channel Sounding TX/SNR (18dB, 21 dB, 24 dB and 27dB)
Channel Sounding PHY 2Mbps BT2.0
Channel Sounding additional supported timings:
T_PM=10us
T_IP1/T_IP2=60, 50, 30
T_FCS=120, 100, 60
LE Power Control (\LEPC).
Additional features supported as EAR (\Early Access Release) in the KW45 / KW47 experimental builds:
LE Test Mode Enhancement (\UTP/OTA).
LL Extended Feature Set
Monitoring Advertisers
Randomized Resolvable Private Address (\RPA)
LE Enhanced Connection Update
Note: Project configuration enabling Experimental features on KW45 and MCX W71 requires the Radio Subsystem (NBU) Firmware to be reprogrammed with the firmware provided in the SDK under \middleware\wireless\ble_controller\bin\experimental\. For NBU programming steps, see the EVK Quick Start Guide and Secure Provisioning SDK (SPSDK) documentation.
Project configurations that require usage of the Bluetooth LE controller including all Bluetooth LE examples require the Radio Subsystem (NBU) Firmware to be re-programmed with the firmware provided in the SDK under middleware\wireless\ble_controller\bin.
Bluetooth LE Host Stack and Applications#
The Bluetooth LE Host Stack component provides an implementation for a Bluetooth 6.0 mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.
Main features supported:
Automotive Compliance
MISRA Compliance
HIS CCM <= 20
Advanced Secure Mode
Enhanced ATT
GATT Caching
GCC Libraries
IAR Libraries
Bluetooth LE Peripheral Libraries
Bluetooth LE Central Libraries
Bluetooth LE Full Host Features Libraries
Bluetooth LE Host Optional Features Libraries
Bluetooth LE Host Mandatory Features Libraries
BareMetal and FreeRTOS Support
Full Privacy Support
NCP Mode - FSCI Application
Enhanced Notifications
Dynamic Database
OTA Support - Sample Applications
Decision based Advertising Filtering (DBAF)
Advertising Coding Selection (ACS)
Periodic Advertising with Responses (PAwR)
Encrypted Advertising Data (EAD)
Monitoring Advertisers - Experimental feature
Randomized RPA - Experimental feature
Intrusion Detection System (IDS) - Experimental feature
Note: The CDE(Complex-domain Distance Estimation) algorithm is an experimental feature intended only for testing purposes. It is not maintained and must not be included in production environments.
Parent topic:Wireless connectivity middleware overview
Wireless Localization#
Localization
Connectivity framework#
The Connectivity Framework is a software component that provides hardware abstraction modules to the upper layer connectivity stacks and components. It also provides a list of services and APIs (see Supported services). The Connectivity Framework modules are located in the middleware\wireless\framework SDK folder.
Supported services#
FSCI - Framework Serial Communication Interface
FunctionLib - Common function library utilities
HWParameter - Hardware parameter management
LowPower - Low power mode management
ModuleInfo - Module information and versioning
NVS - Non-Volatile Storage
NVM - Non-Volatile Memory management
OtaSupport - Over-The-Air update support
SecLib_RNG - Security library and Random Number Generator
Sensors - Sensor abstraction layer
SFC - Smart Frequency Calibration
WorkQ - Work queue management
Supported platform#
KW45_MCXW71
KW47_MCXW72
MCXW23
RW61X
RT1060 and RT1170
i.MX RT595s
Advanced features supported on platforms#
KW45_MCXW71#
FRO32K with smart frequency calibration (see SFC)
Power down mode support (for evaluation only)
KW47_MCXW72#
FRO32K with smart frequency calibration (see SFC)
Power down mode support (for evaluation only)
Crystal 32M trimming with temperature
Debug module for NBU
Extended NBU support with SecLib and pseudo RNG support
CMSIS DSP Library#
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
TF-M#
Trusted Firmware - M Library
PSA Test Suite#
Arm Platform Security Architecture Test Suite
NXP PSA CRYPTO DRIVER#
PSA crypto driver for crypto library integration via driver wrappers
secure_storage#
secure_storage
EdgeLock SE050 Plug and Trust Middleware#
Secure subsystem library - SSS APIs
Multicore#
Multicore Software Development Kit
NXP IoT Agent#
NXP IoT Agent
mbedTLS#
mbedtls SSL/TLS library v3.x
mbedTLS#
mbedtls SSL/TLS library v2.x
LittleFS#
LittleFS filesystem stack
FreeMASTER#
FreeMASTER communication driver for 32-bit platforms.
Release contents#
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
|---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
What is new#
The following updates were implemented with respect to the previous SDK release version (26.09.00-pvw1).
Bluetooth LE Host Stack and Applications
Added
Added
gSecEvt_SameConfirmValue_cIDS event to detect Legacy Pairing Confirm Value replay attacks.
Improved
Replaced mode assert with graceful drop and cleanup in localization applications.
RAS/RAP: handle case where MTU size reduction forces use of more segments than predefined
gRASMaxNoOfSegments_c.Advertising-set-related BLE Host storage is now allocated by the application and scales with the configurable
gMaxAdvSets_c.
Fixed
Fixed Insufficient Encryption returned instead of Insufficient Authentication.
Fixed mismatch between ExtendedFeatures from GAPInit and HCI LE Read All Remote Features Complete event.
Miscellaneous Sample Applications fixes.
Miscellaneous Coverity fixes.
Miscellaneous MISRA fixes.
Details can be found in github repository nxp-mcuxpresso/mcuxsdk-middleware-bluetooth-host/CHANGELOG.md.
Bluetooth LE controller
HADM, PAwR fixes, and stability improvements.
Transceiver drivers (XCVR)
Added support for Bluetooth LE Channel Sounding.
Added API to control Power Amplifier (PA) ramp type and duration.
Connectivity framework
Major Changes
[NVM] Enhanced robustness of NVM MIT (Meta Information Tag) operations with improved validation and error handling. Added checksum validation feature controlled by
gNvmMetaCheckSum_dcompilation switch. Systematically validates MIT fields before use and triggers page switch if corruption detected. FixedmNvTableSizeInFlashtracking when table entries are modified. RefactoredNvWriteRecord()and addedNvModuleSwitchPage()for better ECC fault handling. AddedNvSetChecksumEnable()API to control feature at runtime. The feature is disabled by default.[SecLib_RNG] Refactored SecLib mutex declaration and made Lock/Unlock functions public. Changed return type from
osa_status_ttosecResultType_tfor SecLib mutex functions and moved mutex Lock/Unlock function declarations to SecLib.h.[SecLib_RNG][PSA] Activated PSA opaque execution with s200 and its secure key storage. Switched from PSA transparent mode to opaque mode for all functions except
CMAC_LsbFirstInput()which is currently not supported in opaque version. OptimizedSecLib_psa_configto fully accelerate allPSA_WANT_KEY_TYPE_ECC_KEY_PAIRfunctions.
Minor Changes
[wireless_mcu][ble] Refactored
PLATFORM_SetBleMaxTxPower()API moved from platform file tofwk_platform_ble.cfor Zephyr compatibility.[wireless_mcu] Modified
PLATFORM_GetBDAddr()to return consistent address across calls whengPlatformUseHwParameter_dis disabled.[Common] Enhanced external flash API with C++ compatibility by adding extern “C” guards.
[wireless_nbu] Replaced
FPGA_TARGETguard withFWK_KW43_MCXW70_NBU_FAMILIESfor CPU clock configuration to better reflect target family.[DBG] Disabled DTEST signals and GPIO debug for debug target to prevent significant low power current consumption degradation.
[kw45_k32w1_mcxw71][kw47_mcxw72] Removed use of SIRCCSR SDK definitions for wakeup by UART0.
[platform] Added platform abstraction macros
PLATFORM_GET_IPSR,PLATFORM_SET_INT_MASK, andPLATFORM_CLEAR_INT_MASKto allow platform-specific customization of IPSR read and interrupt mask functions while maintaining backward compatibility.
Bug Fixes
[OTA][Coverity] Sanitized the
pImageOffsetparameter in OTA functions to avoid possible overflow.[SecLib] Fixed multiplication buffer pointer initialization for segmented ECDH operations. Fixed EC P256 multistep operations using SW legacy library. Fixed
ECDH_P256_ComputeDhKeySeg()andECDH_P256_GenerateKeysSeg()argument checking across SecLib variants. FixedSecLib_AES_CMAC_PRF_128()behavior for SecLib sss variant that tolerated VK length to be 0. Removed unreachable code fromSecLib_HMAC_SHA256_Finish().[Platform] Fixed TSTMR timestamp 64 bit read compilation failure when
gPlatformTstmr32Bit_dis undefined.[NVM] Fixed initialization procedure in
InitNVMConfig()to validatestart_addrandpartition_size.[wireless_nbu] Fixed resource access issue by reverting TSTMR read restriction on NBU as underlying issue has been resolved.
[wireless_mcu][wireless_nbu] Fixed timestamp initialization to ensure a defined value when the
tstmrIdis out of range.[SecLib_RNG] Corrected copyright header in
seclib.c.[MISRA] Various MISRA and CERT-C compliance fixes in NVM module.
Known issues#
This section lists the known issues, limitations, and/or workarounds.
FRO6M Clock Stability Issue#
According to ERRATA ERR052742, the FRO6M clock is not stable on some parts. FRO6M outputs lower frequency signal instead of 6MHz when device is reset or wakes up from low power. It can impact peripherals using it as a clock source.
Impact on TSTMR Module#
The TSTMR (Time Stamp Timer) module exclusively uses the FRO6M clock source. Due to the aforementioned stability issues, avoid using TSTMR-related APIs if your application requires high-precision timing.
Recommendation#
For applications requiring precise timing, consider using alternative timer modules that support more stable clock sources.
Maximum file path length in Windows 7 operating system#
The Windows 7 operating system imposes a 260-character maximum length for file paths. When installing the MCUXpresso SDK, place it in a directory close to the root to prevent file paths from exceeding the maximum character length specified by the Windows operating system. The recommended location is the C:\nxp folder.
Only FreeRTOS is tested for RTOS support#
This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.
Bluetooth LE#
Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.
Bluetooth LE controller:#
The maximum Advertising data length is limited to:
800 bytes for KW45/KW47
31 bytes for KW43.
The scanner may sporadically miss some chained packets.
Periodic Advertising with Responses (PAwR):
Periodic Advertising with Response (PAwR) is not supported with the configuration “Subevent Interval = Number of Response Slots x Response Slot Spacing with Response Slot Spacing = 0x2”.
The feature is not functional with the Free-Running Oscillator (FRO32K); it requires a 32 KHz Crystal Oscillator with accuracy less than 50 ppm.
KW43:
CS testmode does not work.
CS works only over 1M ACL connection.
CS performances are not yet guaranteed.
KW45 / MCXW 71: No specific issues.
KW47 / MCX W72: Channel Sounding (CS): Information:
RF Bandwidth Occupancy and Connections/Channel Sounding Activities: The RF bandwidth occupancy is tightly coupled with configured activities, including the number of connections, connection event durations, the number of Channel Sounding (CS) procedures, and related CS parameters (e.g., subevent length, repeat mode). The Link Layer Scheduler is responsible for allocating RF bandwidth to these activities, optimizing bandwidth utilization. However, because each activity operates on its own timing constraints, some RF collisions are expected. This is inherent to the Bluetooth LE protocol, particularly when peripheral roles are configured, as anchor placement is controlled by the central peer devices. The application controls several timing parameters, such as connection interval and subevent length. To optimize user experience, the Link Layer expects the application to adjust these parameters to achieve the best RF bandwidth occupancy with the lowest occurrence of RF collisions.
Limitations:
RTT with Sounding Sequence is not supported.
Maximum 6 Channel Sounding procedures are supported in parallel.
Phase measurement bias is within certification range (<1.7x2πns) with KW47 EVK board. However, if different PCB or antenna matching is used, some bias may appear due to increased delay.
For experimental feature IPT(Inline PCT Transfer), only 1x1 configuration is supported.
Known issues:
When CS Subevents are configured very close from each other (<700us), some Subevents may be aborted with reason 0x3.
When CS offset is configured too close from ACL anchor point, the anchor point may not be served (TX on central or RX on peripheral will not happen). Ideally, CS Offset should be configured greater than 1ms.
RTT bias compensation:
For parts not properly configured at production (IFR blank), RTT bias is not compensated properly. Consequently, an inaccuracy of +/-2m can be observed.
Pairing procedure fails to complete after connection is established. Affects digital_key sample applications. Increase
gHost_TaskStackSize_cto1900U.Channel Sounding measurement cannot start after handover. Affects digital_key sample applications.
Other limitations#
The following Connectivity Framework configurations are Experimental and not recommended for mass production:
Power down on application power domain.
GenFSK
Connectivity_testapplication is not operational with Low Power enabled.Serial manager is only supported on UART (not I2C nor SPI).
If the FRO32K is configured as the clock source of the CM33 Core then the debug session will block in IAR CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.
In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.